Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Product List
Fundamentals of Oscilloscopes Slide 20

Acquisition memory is another very important topic. Typically it is specified in points, kilo points or mega points. It is memory per channel, plus in some oscilloscopes users can interleave channels to double up on the memory. Memory size defines acquisition time. For example, with a 1 GS/s sample rate and 20,000 points of memory, with a little bit of math the result is a 20 µs capture window. There is a memory sequencing mode that allows the user to optimize the memory for capturing very fast signals where is a need to digitize rapidly and that have large signal gaps or long dwell times between the events. This allows the user to not waste memory, for example if they were capturing a 20 ns pulse every two seconds.

PTM Published on: 2012-06-11