Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Product List
Fundamentals of Oscilloscopes Slide 16

The main purpose of an oscilloscope is to analyze and view analog waveforms. To do this, the oscilloscope samples a waveform at some finite sample rate, generating a vector of voltages with respect to time. Since this vector represents a set of points (not the actual smooth analog waveform), it is often desirable to modify the acquired waveform by generating samples that are predicted between the actual acquired points. The generation of samples that occur in between actual waveform samples is called interpolation. When done properly, this results in a waveform with a higher resultant sample rate that is a closer approximation of the analog waveform under analysis.

PTM Published on: 2012-06-11