Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Product List
Fundamentals of Oscilloscopes Slide 18

The next waveform display topic is measurements and statistics. Modern scopes have the ability to display measurements such as frequency, period, rise time, and fall time. This can be very useful in debugging electrical designs, giving the user additional insight into the circuit being tested. Some statistics may be seen on screen as well, including the minimum, the maximum, as well as the standard deviation and the mean value based on the number of measurements. LeCroy also does “All Instance Measurements”. For example, if there are nine rise times in the capture window and the rise time is measured, the mean value is the result of all nine rise times.

PTM Published on: 2012-06-11