Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Overview-Slide8

The second set of 20-pin options (R8C/28,29 and 32x) is shown here. At the peripheral-level, the devices are fully compatible, which is again one of the greatest strengths of the R8C family. However, looking closer at the specifications, there are some key differences between the 2x and 3x series. Examples of this include the addition of a DTC (Data Transfer Controller), extra I²C, and a larger RAM-to-ROM ratio in the 32x.

PTM Published on: 2012-01-03