Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Overview-Slide11

Here are the details of the R8C/2G and 26-27 groups. Note that there are a few additional blocks in the 26, 27 group. Both options have a 16-bit timer, but the Timer RC in the 26, 27 provides additional features not available in Timer RF. Other key differences are Data Flash, RAM size, and an external main clock. As part of the low-end R8C line-up the R8C/2G has been optimized for cost, while providing adequate functionality and I/O input to output for simpler applications.

PTM Published on: 2012-01-03