Using the voltage program feature, the output voltage of the GWS250 can be adjusted over a wide range, as shown on this slide. The bottom right hand graph shows the external voltage level required to program the output. For example, to set the output voltage of the GWS250-24 to 28.8V, apply 6V to the "PV" terminal.