Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
ML610Q100-Slide16

These devices have four channels of 16-bit PWM control. Three channels have one output each and the fourth has three outputs that can operate synchronously to one another. The three channels of PWMF, the fourth PWM module, can each have different duty cycles, as can all of the three other PWM outputs. There are multiple interrupt sources for each PWM module. Each PWM has an Emergency STOP and Emergency STOP interrupt.

PTM Published on: 2014-06-09