Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Family-Slide6

The diagram on the left shows the pin assignment in the R8C/3x Series. The colored circles depict the location of ports and system pins. Besides having the same CPU core and same peripherals, these devices have been carefully designed to provide 100% package scalability. As shown in the diagram on the right, the R8C comes in packages as small as 4mm x 4mm to 16mm x 16mm. By providing such scalability and compatibility, designers can easily tackle two great challenges: migration up or down in case the application’s requirements change, and providing designs for multiple versions of the product by incorporating multiple package footprints. Renesas’ ultimate goal is to enable designers to reduce time-to-market and total development cost.

PTM Published on: 2012-01-03