Pico Inventor's Kit Experiment 7 - Seven Segment Display
2025-10-16 | By Kitronik Maker
Courtesy of Kitronik Maker
Guide by Kitronik Maker
Experiment 7 from the Inventors Kit for Raspberry Pi Pico, in which we explore using a seven segment display. Included in this resource are code downloads, a description of the experiment and also a video walk-through. This resource provides additional help and is not meant to replace the documentation that ships with the kit.
The Raspberry Pi Pico is a compact microcontroller based on the RP2040 processor - Raspberry Pi’s first in-house designed silicon. The RP2040 on the Pico uses 2 ARM processor cores, and also has 4 programmable IO controllers (PIO). These are like mini processors, and can help the Pico complete more complex tasks than it would otherwise be able to do. The Pico has 28 general purpose IO pins (GPIO), and 3 of these can also be used as Analogue inputs. The Pico can be programmed in several languages. The experiments in these resources are written in the Thonny Editor using MicroPython.
Pico Inventor's Kit Exp' 7 - Seven Segment Display
Seven segment displays are a great way of showing numerical values. Each element can be controlled independently. As the name suggests there are seven elements that can be controlled, plus a decimal point (making eight in total). In this experiment we will control the elements to make the display count from zero to nine and back down to zero again.
- To learn how individual segments in a seven segment display are controlled.
- To make the display count from 0 to 9 and back to 0 again.
Exp 7 - The Code
All experiments are coded in MicroPython in Thonny. To open in Thonny, copy and paste the code below directly into the Thonny editor.
'''
Kitronik Inventor's Kit Exp 7
Control a seven segment display.
Count up from 0 to 9 and then back again.
'''
import machine
import time
segA = machine.Pin(18, machine.Pin.OUT)
segB = machine.Pin(17, machine.Pin.OUT)
segC = machine.Pin(16, machine.Pin.OUT)
segD = machine.Pin(15, machine.Pin.OUT)
segE = machine.Pin(14, machine.Pin.OUT)
segF = machine.Pin(13, machine.Pin.OUT)
segG = machine.Pin(12, machine.Pin.OUT)
pins = [segA, segB, segC, segD, segE, segF, segG]
'''
This list of 10 numbers shows the states of the pins for the segments
to display the appropriate number. This is used to simplify the code
later - we can index the list to display the correct number.
'''
# numbers = [zero, one, two, three, four, five, six, seven, eight, nine, clear display]
numbers = [[1,1,1,1,1,1,0],
[0,1,1,0,0,0,0],
[1,1,0,1,1,0,1],
[1,1,1,1,0,0,1],
[0,1,1,0,0,1,1],
[1,0,1,1,0,1,1],
[1,0,1,1,1,1,1],
[1,1,1,0,0,0,0],
[1,1,1,1,1,1,1],
[1,1,1,0,0,1,1],
[0,0,0,0,0,0,0]]
clearDisplay = 10 # The position in the 'numbers list of the clear display setup
# This function takes in which number should be displayed, and then selects the correct pin/segment setup from the numbers list to control the output pins
def displayNumber(numberToDisplay):
pin = 0
for segment in range (7):
pins[pin].value(numbers[numberToDisplay][segment])
pin += 1
return numberToDisplay
# Loop round displaying 0 - 9 - 0, clear, and repeat
while True:
for i in range(10):
displayNumber(i)
time.sleep_ms(600)
for i in range (9, -1, -1):
displayNumber(i)
time.sleep_ms(600)
displayNumber(clearDisplay)
time.sleep_ms(1000)
Inventors Kit Extra Resources:
Each of the ten experiments has been designed to ease you into coding and physical computing for the for the Raspberry Pi Pico. The experiments have been chosen to cover the key concepts of physical computing and they also increase in difficulty as you progress. This resource has been put together to provide additional information for this experiment and has not been designed to replace the booklet. The majority of the information you will need to perform and understand this experiment is contained in the booklet.
If you are new to coding and physical computing, even the least complex examples can be quite challenging. With this in mind, we created walk-through videos for each of the experiments. Our presenter talks you through the circuit in a way that backs up the information given in the booklet but in a style that some might find easier to absorb. As well as having a video walk-through, each page also contains the code. Although it is always good to tackle the code yourself, it can be handy for testing your circuit quickly. The code has been heavily commented as an extra learning resource. To get the most out of the experiment, once you've tested your circuit have a go at coding the experiment from scratch.
Follow the links in the table below:
| Exp No#. | Experiment Name. |
|---|---|
| 1 | Digital Inputs & Outputs. |
| 2 | Light Sensor & Analog Inputs. |
| 3 | Dimming an LED using a potentiometer. |
| 4 | Using a transistor to drive a motor. |
| 5 | Control a servo with a potentiometer. |
| 6 | Setting the tone with a piezo buzzer. |
| 7 | Using a seven segment display. |
| 8 | Exploring wind power. |
| 9 | Capacitor charge circuit. |
| 10 | Controlling ZIP LEDs. |
©Kitronik Ltd – You may print this page & link to it, but must not copy the page or part thereof without Kitronik's prior written consent.