Maker.io main logo

DC Motor featuring 4Duino-24

18

2016-10-08 | By 4D Makers

License: None Arduino

In this project, we will learn how to control the speed and direction of a DC motor via I/O ports with PWM output capability, a L293D quad half-h drivers IC and 4D Workshop widgets.

In its simplest form, a DC motor has two wires which are connected to a power supply. Depend on whichever way current flows in the DC motor, this will determine the direction in which the motor will spin.

Motors are often used in conjunction with a motor driver to allow speed and direction control via a microcontroller. To fully explain the functionality of the motor driver, we will have a look at a screenshot of the datasheet below. (From Texas Instruments)

Pin Configuration and Functions

There are four input and output channels in the IC itself (1A, 1Y makes one channel). To drive a motor in forward and reverse we would require the use of two channels. You would use the #A pins to input signals from your microcontroller to the driver, while the #Y pins will output an amplified signal. The EN pins are used to open and close two channels at one time, and their main purpose is to stop any currents going to the motor completely. The EN pin in this project will be connected to a PWM enabled pin on the 4Duino to control the speed of the motor.

How it works
How it Works
Components
  • 4Duino
  • 1 x DC motor rated between 4.5V – 12V (N20 Micro Metal Gear Motor used in this project)
  • 1 x L293D IC
  • Jumper cables
  • AA batteries (about 4 – 6 will be sufficient)
  • Battery holder
  • Micro USB cable
  • µSD card
Implementation
Step 1: Build

Build the circuit as shown in the following diagram and schematic.

Circuit Diagram

Step 2: Program

Workshop 4 – 4Duino Basic Graphics environment is used to program this project.

This project requires the Arduino IDE to be installed, as Workshop calls the Arduino IDE for compiling the Arduino sketches. The Arduino IDE, however is not required to be opened or modified to program the 4Duino.

DC_Motor_Driver

Open this file using Workshop 4.

Step 3: Comms Port

Connect the 4Duino to the PC using µUSB cable.
Then navigate to the Comms tab and select the Comms port to which the 4Duino connected.

Step 4: Compile and Upload

Finally, go back to “Home” tab and now click on the “Comp’nLoad” button.

The Workshop 4 IDE will prompt you to insert a micro SD card to the PC in order to save the widget images. Insert micro SD card, select the appropriate drive and press button “OK”.

If the SD card has the widget images you can click button “No Thanks”

Step 5: Insert micro SD card

After uploading the program in to the 4Duino, it will try to mount the µSD card. If the µSD card is not present it will prints an error message. Once µSD card is mounted, you will see the screen displayed in the image on the right. 

DC Motor featuring 4Duino-24

All you need to do is insert the micro SD card you saved the image files into the 4Duino.

Now using the touch sliders on the 4Duino Display, you can control the speed and direction of the motor.

Control the Speed and Direction of the Motor

製造商零件編號 4DUINO-24
4DUINO ATMEGA32U4/ESP8266/PICASO
4D Systems Pty Ltd
製造商零件編號 SK-4DUINO-24
4DUINO ATMEGA32U4/ESP8266/PICASO
4D Systems Pty Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.