Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Grace Software Graphical User Interface Slide 8

Shown on this slide is an example of some Grace™ generated C code. It is fully-commented, and looks just as it would if a programmer had written it line by line. As can be seen, the code is inserted directly into the active project as a C file. Each enabled peripheral has its own C file that is created and integrated directly into the CCS project. Once the device is fully enabled and configured, the application layer can call these enable and initialization functions that Grace generated.

PTM Published on: 2011-12-05