Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
composition
The three basic cable types are multiconductor, multipair, and coaxial. Generally, a cable consists of two or more insulated conductors bundled together where color-coded insulation is used to identify one conductor from another. Coaxial cable, on the other hand, uses a central conductor with an outer braided shield as the return path.
PTM Published on: 2008-08-12