Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List Associated Content
Slide12

Without matching circuits, performance of the antenna at 2.45 GHz is good, as shown in figure (a).  With matching circuits, shown in figure (b), the Return Loss is enhanced (meaning improved VSWR) and the Bandwidth is broadened – both of which are key parameters in improving the overall gain performance of the antenna over the desired frequency.  Note that the matching circuit component values will be different in every application depending on PCB material, thickness, and the factors mentioned earlier.  The values shown are for the Johanson test boards and are good starting values for finding the optimum values for an individual application.