Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List Associated Content
MIPI Kit Demo: Dual-Camera Application

Displayed here is the Dual imaging demo, using both receive and transmit of both controllers on the T20 device. This demo is somewhat similar to the Raspberry Pi demo, but with two instantiations. It includes two cameras connected to the receive channels of the T20 and the transmit channels connected to two different Raspberry Pi boards. When the button is pressed on the board, the two CSI streams will internally switch to the other CSI TX port, thereby switching the images being displayed on the two Raspberry Pi boards/displays. Additionally another button controls use of a Sobel filter showing some basic inline processing function being applied to the video streams. This shows that each of the two Receive and two Transmit channels can all be used simultaneously with in line processing, which is a unique capability for the Trion® devices compared to other device solutions.

PTM Published on: 2020-03-31