Alorium’s XLR8 and Snō dev boards provide yet another simple and inexpensive way to make use of an FPGA’s real-time abilities in embedded system designs.
Integrating machine learning and decision tree processing into IMUs can offload real-time position and movement processing from the host application processor.
Single board computers speed embedded system development.
Don’t wait for 5G: Ready-made 4G LTE modules and associated development kits simplify remote IoT product development and shorten time to market, now.
Adafruit’s CircuitPython brings the increasingly popular Python programming language to inexpensive, embedded microcontroller dev boards.
The HP 9878A I/O expander used switching power supply ICs that are still available today, but practitioners of the art now have a lot more resources available.
IMU software determines precise position from IMU sensor data and is used in embedded applications ranging from consumer to industrial, medical, and military.
Funnel amplifiers allow high side current measurements in systems where the load’s power supply operates at a higher voltage than the measurement circuitry.
Thermal paste has withstood the test of time, but there many new thermal compounds in form factors that make it easier to get the heat out in tricky situations.
Both Zener diodes and voltage references can play important roles in modern circuits.
Integrated time of flight (ToF) sensors provide a simple, fast, and inexpensive way to measure distance and to recognize simple gestures in embedded systems.
The Arduino MKR Vidor 4000 provides a simple and inexpensive way to make use of an FPGA’s real time abilities in embedded system designs.
How to accurately and safely amplify the low-level voltage generated by current sense resistors into a relatively large voltage that’s more easily measured.
Feature-rich, low-cost microcontrollers provide near ideal solutions for numerous embedded applications.
Current sense resistors are widely used to measure current flow to track system performance, but there are nuances to be aware of for successful implementation.
The right tools and techniques make a big difference when it comes to hand soldering electronic components.
IMUs provide precise positioning information for embedded applications ranging from consumer to industrial, medical, and military.
Implement real-time clock/calendar (RTCC) functions in embedded systems with minimal design time, component count, and power consumption.
Some tools are just plain useful: The DigiKey 12-inch ruler is one of them, along with the Aven headband magnifier.
Using the Red Pitaya Open Instrumentation Platform and an array of open development tools, developers can create their own test and measurement systems.