Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
MOSFET-Slide13

The advantages of these MOSFETs include: the same land pattern as standard D-PAK packages, but with a higher rated current; lower RDS(on); and lower heat generation. The circuit examples shown here illustrate a couple of applications (an LCD inverter and a motor drive) for which these devices would be an ideal solution.

PTM Published on: 2012-01-13