Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
Core-Slide11

In summary, the 100MHz on-chip memory means the RX CPU can run full speed with no delays from on-chip memory, the pre-fetch queue minimizes delays when the CPU accesses slower memories, and the RX CPU is the sole master of Internal Main Bus 1. Next this module will look at Internal Main Bus 2.

PTM Published on: 2012-05-15