Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
MMA845xQ-Slide8

To perform orientation detection the interrupt alerts of a sensor change in orientation depending on the configuration selection. By reading the TILT register, the updated orientation is available. Note: up/down/left/right are mutually exclusive from each other, only one can occur at once. However, back/front can occur in conjunction with up/down/left/right. For example, the device can be front/up and then transition to front/right.

PTM Published on: 2012-08-17