New Product Discoveries – Binho and Efinix
In this episode of New Product Discoveries, we are doing things a little differently. Instead of covering two new products, we are featuring two manufacturers that are new to DigiKey's lineup.
The first is a company called Binho. This company is comprised of engineers, inventors, and designers that see a need for a product and create it.
Their products started with, and center around, the Nova Multi-Protocol USB Host Adapter. The other three products currently available allow for this adapter to interface with existing projects using a 2 x 5 pin 2.54 mm pitch connector, Adafruit Feather form-factor devices, and Qwiic Connect System devices.
The second is a company called Efinix. This company has brought an innovative new FPGA technology into the industry. Efinix’s Trion FPGA Silicon Platform uses quantum core fabric that is more easily configurable than traditional FPGAs with fewer metal layers, easing the quantum core integration process.
All the products and supporting products mentioned here are in-stock and available from DigiKey for same-day shipping.

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.
Visit TechForum