How to Ensure Embedded System Security Using DSCs and MCUs
Contributed By DigiKey's North American Editors
2023-07-25
With the migration to the Internet of Things (IoT), security has moved well beyond an optional feature in embedded applications, evolving into a must-have capability that is required to ensure system integrity. To respond to a growing array of security specifications, developers require solutions that not only match application requirements for low power or high performance, but can also deliver hardware-based security capabilities, including authentication, encryption, secure storage, and secure boot.
This article provides a brief introduction to embedded security principles. It then shows how developers can use Microchip Technology’s high-performance digital signal controllers (DSCs) and low-power PIC24F microcontroller units (MCUs), along with Microchip’s specialized security devices, to meet the emerging demand for stringent embedded security.
Embedded security builds upon four key principles
Connected to the public Internet, smart products can be tied together in sophisticated applications that few standalone products can match. However, the threat of cyberattacks using those same connectivity pathways not only potentially limits the value of smart products, but also exposes those products, the associated applications, and their users to seemingly endless sources of threats.
Besides facing continued consumer demand for system-level cybersecurity, developers increasingly need to address security specifications from national and regional organizations. Two of the most influential specifications, Europe’s ETSI EN 303 645, “Cyber Security for Consumer Internet of Things: Baseline Requirements,” and the United States’ NIST IR 8259, “Foundational Cybersecurity Activities for IoT Device Manufacturers,” suggest cybersecurity practices depend upon four key principles:
- Use of unique passwords
- Availability of secure storage on the device for sensitive security parameters
- Secure communication through mutual authentication and encrypted communication
- Ability to ensure firmware integrity and authenticity through secure boot and secure firmware update
Delivering systems based on these core principles requires the use of a trusted platform that prevents hackers from injecting compromised code that alters communications, storage, firmware, or even security mechanisms themselves.
Trusted platforms help ensure security by building system-level security from the ground up using immutable hardware-based security mechanisms. Although straightforward in concept, implementation of system-level security has been challenging because a security weakness in any part of the system can provide an avenue for cyberattack. By using Microchip Technology’s high-performance dsPIC33C DSCs and low-power PIC24F MCUs, in combination with Microchip’s companion security devices, developers can more easily implement embedded designs that ensure system-level security.
Meeting performance and power requirements
Designed to support a wide range of use cases, devices in Microchip’s dsPIC33C DSC and PIC24F MCU families each combine robust execution platforms with application-specific capabilities, including an extensive complement of integrated analog, waveform control, and communications peripherals. In fact, using the multiple pulse-width modulation (PWM), programmable gain amplifiers (PGAs), analog-to-digital converters (ADCs), and other peripherals on a dsPIC33C DSC, developers can implement complex systems with a minimum of additional components – typically needing only the power devices required in any such design. An example is the use of the DSPIC33CK512MP608 single-core DSC to implement an offline uninterruptible power supply (UPS) design (Figure 1).
Figure 1: As with other dsPIC33C DSCs, the DSPIC33CK512MP608 single-core DSC integrates a comprehensive set of peripherals, simplifying the design of complex systems such as the offline UPS shown. (Image source: Microchip Technology)
For applications that require both real-time control capabilities and digital signal processing, dsPIC33C DSCs combine the capabilities of an MCU and a DSC with its specialized instructions and hardware functionality. For safety-critical designs, dsPIC33C DSCs are IEC 60730 functional safety ready and ISO 26262-compliant, providing multiple hardware features designed to simplify functional safety certification for Automotive Safety Integrity Level B (ASIL-B), and SIL-2 automotive and industrial safety-critical applications.
While dsPIC33C DSCs are designed for applications where performance is paramount, PIC24F MCUs provide a balance between performance and power efficiency for general-purpose embedded systems, consumer electronics, industrial automation, medical devices, and other applications that require control and connectivity but do not need DSP capabilities. As with dsPIC33C DSCs, PIC24F MCUs are IEC 60730 functional safety ready devices with Class B safety diagnostic libraries for building household applications.
As noted earlier, firmware integrity is a core principle of embedded cybersecurity. To help developers ensure firmware integrity and overall code protection, Microchip provides Flash one-time programmable (OTP) by in-circuit serial programming (ICSP) Write Inhibit and CodeGuard Flash security in dsPIC33C DSC devices, such as the DSPIC33CK512MP608 single-core DSC and the DSPIC33CH512MP508 dual-core DSC, as well as PIC24F MCU devices such as the PIC24FJ512GU405 MCU, among many others configured with different sets of application-specific peripherals.
Protecting device firmware
Flash OTP by ICSP Write Inhibit enables developers to configure portions of Flash memory as OTP memory and to read/write protect the Flash memory. Microchip’s proprietary ICSP capability permits these devices to be serially programmed through a pair of pins while running in the end application. With this capability, manufacturers can complete programming on production boards. While ICSP requires use of an external programming device to control the Flash OTP process, Enhanced ICSP allows an on-board bootloader to control the Flash OTP process. These devices also support run-time self-programming (RTSP), which allows the Flash user application code to update itself during run time.
After programming their production device, developers can activate ICSP Write Inhibit, which prevents any further ICSP programming or erasure. Nevertheless, RTSP Flash erase and programming operations can proceed even when ICSP Write Inhibit is activated if appropriate Flash-update code is programmed into the device prior to its activation. As a result, developers can use a trusted bootloader to alter Flash even when ICSP Write Inhibit is activated, allowing them to securely update firmware while still mitigating external attempts to update Flash in production systems.
CodeGuard Flash security provides fine-grain protection of program Flash through the use of separate boot and general segments. Developers define the size of these segments by setting the address of the boot segment (BS) limit (BSLIM) in the device’s BSLIM register; the general segment (GS) occupies the remaining memory. To further protect sensitive information, each segment contains additional partitions. For example, the BS contains the interrupt vector table (IVT), the optional alternate interrupt vector table (AIVT), and additional instruction word (IW) space; the configuration segment (CS), which contains critical device user-configuration data, lies within user address space in the GS (Figure 2).
Figure 2: The dsPIC33C DSC and PIC24F MCU families support code protection in separate partitions such as the BS and GS. (Image source: Microchip Technology)
After setting segment partitions, developers can use the device’s firmware security (FSEC) register to optionally enable write protection and set the required code protection level for each segment. During runtime, the device prevents code contained in a segment with a lower code-protection level from accessing code contained in a segment with a higher code-protection level. In a typical system, developers would write protect the BS and set its code protection to a high level, mitigating external attempts to alter the BS, including the bootloader.
Implementing secure over-the-air firmware update
Software developers are inevitably faced with the need to update software in response to the combination of newly discovered software bugs, competitive enhancements, or emerging security threats. Unlike mobile app updates, performing secure updates to firmware in embedded systems risks interfering with currently running applications at best, or “bricking” the system at worst. Microchip’s dsPIC33C DSCs and low-power PIC24F MCUs families provide a dual-partition mechanism designed to help developers avoid these problems.
In standard operating mode, these devices use all available physical memory as a continuous, single-partition memory space (Figure 3, left) that can be configured into separate BSs and GSs. In dual-partition mode, developers split physical memory into separate active and inactive partitions (Figure 3, right).
Figure 3: Developers can operate the dsPIC33C DSC and PIC24F MCU families in the default single-partition mode or in the dual-partition mode. (Image source: Microchip Technology)
Operating in dual-partition mode, these devices can continue executing application code in the active partition while programming the inactive partition. After programming has been completed, execution of the boot swap (BOOTSWP) runtime instruction causes the device to switch the boot target to the updated partition. If the code in the updated partition fails or is otherwise found deficient, a device reset will automatically cause the device to boot into the original partition (Figure 4).
Figure 4: In dual-partition mode, the dsPIC33C DSCs and PIC24F MCUs can load application code in one partition while continuing to execute application code in the other partition. (Image source: Microchip Technology)
After the success of the updated partition is assured, the flash boot sequence (FBTSEQ) of the updated partition can be set to a lower value than the original partition. On subsequent device resets, the device will boot into the updated partition with the lower FBTSEQ value (Figure 5).
Figure 5: Dual-partition mode allows developers to specify the sequence for booting into the desired partition following device reset. (Image source: Microchip Technology)
Flash OTP by ICSP Write Inhibit and CodeGuard Flash security provides critical support for static and runtime code security, but comprehensive embedded security requires additional mechanisms, including secure key storage, code authentication, and secure communications.
Using companion security devices to ensure embedded system security
By combining dsPIC33C DSCs and PIC24F microcontrollers with Microchips’ ATECC608 CryptoAuthentication or the TrustAnchor100 (TA100) CryptoAutomotive security IC, developers can more easily deploy the full complement of hardware-based security capabilities.
These security ICs provide hardware-based tamper-resistant security mechanisms, including secure storage, hardware-accelerated cryptography engines, true random number generators, and other mechanisms required by cryptographic algorithms. Designed specifically as companion devices, the ICs can be easily added to DSC or MCU system designs to complete the implementation of full embedded systems security (Figure 6).
Figure 6: Security ICs such as the ATECC608 or TA100 complement the security features of the dsPIC33C DSCs and PIC24F MCUs, simplifying the implementation of secure embedded systems. (Image source: Microchip Technology)
Execution of a critical operation like secure firmware update illustrates the complementary security features of dsPIC33C DSCs and PIC24F microcontrollers in conjunction with these companion security ICs. Developers use code-signing techniques to verify the authenticity and integrity of code prior to completion of firmware update operations. Here, developers use their development systems to create an update package containing the code, code metadata, and a signature used for verification (Figure 7).
Figure 7: Code signing provides a vital protocol routinely used to verify the authenticity and integrity of code prior to update on a target system. (Image source: Microchip Technology)
On the target system, hardware-based signature verification eliminates the risk of compromised verification protocols that was possible with the kind of software-based signature verification used in the past. Instead, a companion security IC such as Microchip’s ATECC608 and TA100 rapidly and securely performs signature verification operations without risk of compromise (Figure 8).
Figure 8: In a target system, hardware-based verification provided by a security IC such as the ATECC608 or TA100 is essential for ensuring verification of code prior to firmware update by the bootloader. (Image source: Microchip Technology)
To accelerate the implementation of secure systems, Microchip provides a combination of software and hardware development tools.
Speed software and hardware development
While the MPLAB X integrated development environment (IDE) provides developers with a full software development environment, the MPLAB XC C compiler provides development support for existing tool chains. To speed development in either environment, the Microchip MPLAB Code Configurator (MCC) lets developers use a graphic interface to automatically generate initializers, build drivers, allocate pins, implement libraries, and otherwise help speed many of the critical low-level setup procedures and processes associated with any embedded software development project.
To speed the implementation of a suitable secure bootloader, Microchip’s Bootloader for dsPIC33 DSCs and PIC24 MCUs provides a graphical interface that helps developers quickly configure and generate the custom bootloaders required for their application. A related bootloader host application further simplifies the transfer of application code to the target device.
For hardware development, Microchip provides several associated development boards for building systems based on dsPIC33C DSCs or PIC24F MCUs. In fact, Microchip’s PIC-IoT Board EV54Y39A and PIC-IoT Board AC164164 (Figure 9) integrate security ICs that are pre-provisioned with security credentials for Amazon Web Services (AWS) and Google Cloud, respectively.
Figure 9: Boards such as the PIC-IoT Board AC164164 help accelerate embedded security development by integrating security ICs that are pre-provisioned with credentials for AWS or Google Cloud. (Image source: Microchip Technology)
For custom designs, Microchip offers a dsPIC33CH Curiosity development board (DM330028-2) based on the dsPIC33CH512MP508 dual-core DSC. Alternatively, developers can attach Microchip’s dsPIC33CH128MP508-based plug-in module (MA330040) to a Microchip Explorer Embedded Evaluation Board (DM240001-2) to speed the development of secure embedded systems.
Conclusion
Embedded system security relies on the availability of hardware-based mechanisms, able to support core cybersecurity principles that include firmware integrity, authentication, encryption, and secure storage. While Microchip’s dsPIC33C DSCs and PIC24F MCUs simplify code protection, its ATECC608 and TA100 security ICs provide the additional security mechanisms required in an effective security platform. Using these devices in combination, developers can meet the need for system-level security in embedded solutions for the IoT, as well as automotive, industrial, consumer, and medical applications.

Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of DigiKey or official policies of DigiKey.