SMD Resistor Code Calculator

The surface mount resistor code calculator can be used to determine the resistance value of an SMD resistor using the markings found on the device. Choose the code format: three digit EIA, four digit EIA, or EIA-96. Then select the markings.

Resistor Code Format

Standard-tolerance SMD resistors use a 3-digit code to mark the resistance value on the part. The first two numbers will indicate the significant digits, and the third will be the multiplier. 'R' is used to indicate the position of a decimal point.

Similar to the three digit EIA, the four digit format uses the beginning values to indicate the significant digits while the last digit is the multiplier. 'R' is used to indicate the position of a decimal point. The four digit format allows for higher precision.

The EIA96 system of part marking is based on the EIA96 series of standard resistor values and is typically used on 1% tolerance parts. It uses three characters (two numbers and a digit) in which the numbers represent the value (34 = 34th value of the possible range) and the letter represents the multiplier.

Invalid code
Invalid code
Invalid code