Telematics Enabling Fault Diagnostics for Engines

By Tawfeeq Ahmad

Contributed By DigiKey's North American Editors

Diesel engines are critical system components in a majority of applications ranging from industries, mining, healthcare, construction, datacenters, banks, and utilities. Fault occurrence and downtime in the engines can lead to a monetary impact. Hence, there has been an increased adoption of smart monitoring solutions for diesel engines.

Why is telematics required for engines?

As the monitoring and maintenance of diesel engines have always been manual and onsite, it results in heavy losses for industries, rental agencies, and customers due to lack of relevant data. Telematics for diesel engines ensures uninterrupted operation.

Telematics provides visibility on various parameters such as engine power, fuel consumption, location and hours of usage. Insights on these parameters can help with optimizing maintenance schedules and preventing generator service outages. Telematic can also support further analysis through software that provide predictive analytics, user alerts, intelligent dispatching, and many other valuable features. With the help of these powerful metrics, users and businesses can create significant savings, have a higher return on investment (ROI), and improve customer service.

Diagnostics data for engines

Telematics devices pull the data from the onboard diagnostics system to provide valuable information on machine health, performance, and status. Diagnostic information includes fuel consumption, engine run time and the power status.

Typically, the results of this data reach the user in easy-to-read software systems, many of which can be accessed from any device. In addition to sending data online, smart telematics solutions send reports via SMS notifications on detected events (Figure 1). Some of the challenges that telematics solutions can solve consist of scheduling maintenance and stolen equipment recovery.

Image of some of the events that can be detected and relayed to appropriate personnelFigure 1: Some of the events that can be detected and relayed to appropriate personnel for action if needed. (Image source: iWave Systems)

Few reasons why a smart monitoring solution is necessary for engine manufacturers:

  • Streamline performance by continuously monitoring vital parameters across the deployment sites
  • Improve decisions by accurate detailed insights and real-time analytics of diesel engine performance
  • Enhance customer satisfaction by proactively addressing issues before they become problems
  • User-defined SMS alerts for engine faults and misuse
  • Classification of information (region wise / model wise / dealer wise)
  • Higher profit by tracking the fuel consumption, fuel theft, and unauthorized usage. There is also a reduction in operational costs as there is no manual dependency

Importance of rugged telematics hardware

Diesel engines work in tough conditions and demanding environments. To track engines effectively, users need a telematics solution that is built to operate where engines are located and work in the same difficult conditions.

To connect to the engines, the telematics hardware is integrated with connectivity options such as CAN, RS232 and RS485. Based on the installation area, there are also different wireless connectivity options to be considered such as LTE Cat-4, LTE Cat-M1 and Wi-Fi.

A ruggedized telematics device is designed for harsh outdoor environments common in industrial, heavy-duty and utility applications. The telematics device features a rugged exterior enclosure that allows for installation outside while withstanding shaking and shock. The device is designed according to the international standard IP67 strengthened to withstand intrusion of solids, dust, accidental contact, cold and water.

iWave hardware for diesel engines monitoring

Our innovative portfolio of telematics solutions and protocol stacks are designed to work with any engines to remotely monitor vital aspects and provide real-time information on key parameters. The rugged telematics device from iWave Systems can be installed along with the intelligent sensors on the diesel engines that monitor various parameters such as fuel consumption, diesel engine run hours, fuel refills, health, battery voltage, coolant level, pressure, temperature, and energy for a seamless operation.

Diagram of sensors on the diesel engine send their data to iWave’s telematics device (click to enlarge)Figure 2: Sensors on the diesel engine send their data to iWave’s telematics device which then relays it to the web for users to access. (Image source: iWave Systems)

The sensors communicate with iWave’s gateway device which then transmits these readings to a server or the cloud over the internet (Figure 2). The sensors monitoring the diesel engines work on 4G wireless technology. Through user interactive web and mobile applications, engine parameters can be viewed in real time and can create reports anywhere and anytime. A remote monitoring platform allows users to monitor the equipment 24×7 across multiple locations addressing the challenges.

The SAE J1939 protocol stack is used to collect the parameters from diesel engines. iWave has developed the stack based on the ANSI C standard supporting all the specifications of the SAE J1939 protocol needed for collecting data from diesel engines. The stack works with an extended 29-bit CAN identifier with all the standard baud rates (100 kbps, 125 kbps, 250 kbps, 500 kbps, and 1000 kbps) supported.

The telematics gateway device interfaced with diesel engines provides the following benefits:

  • Monitoring a range of important parameters related to engines
  • Option to add additional sensors
  • Secured data storage and analytics capabilities
  • Preventing fuel thefts
  • Monitoring the machine run time
  • Record fuel consumption and draining
  • Emergency fuel balance

iWave offers a fully scalable solution to monitor and diagnose entire engine from anywhere, anytime assuring user peace of mind. Our predictive technology makes sure that your generators are in good and healthy condition to function uninterruptedly in an event of an emergency and prevent fuel thefts and generator breakdown.

DigiKey logo

Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of DigiKey or official policies of DigiKey.

About this author

Image of Tawfeeq Ahmad

Tawfeeq Ahmad

A strong interest in product marketing coupled with a passion for IoT and Wireless Solutions, Tawfeeq specializes in building connected mobility solutions and Industrial IoT Solutions. With data being the new money, there is a dependency for rugged gateways and innovative hardware. Tawfeeq likes to help companies in their transformation journeys.

About this publisher

DigiKey's North American Editors