How to Design a Modular Overlay Network for Industry 4.0 Data Processing Optimization in the IIoT
Contributed By DigiKey's North American Editors
2022-05-04
Data processing optimization in Industry 4.0 and the Industrial Internet of Things (IIoT) systems to support lean manufacturing can be accomplished through condition monitoring, predictive maintenance, overall equipment effectiveness (OEE) analysis and tracking, diagnostics, and troubleshooting. The problem in many instances is that legacy equipment was either not designed to be connected or may use any of a number of a variety of communications protocols, making it expensive to replace them all. To ensure maximum effectiveness and obtain actionable machine data, it’s simpler and more cost-effective in many instances to implement an overlay network that can connect existing automation islands and legacy equipment.
Designing such an overlay network is a challenging undertaking. It requires a controller that can receive signals from sensors and other devices that use a variety of communications protocols, combine those signals into a unified stream of useable data, and export that data to edge computing resources or the cloud. The system needs adapters that can connect directly to sensors, indicators, and other devices. Converters are needed to connect previously incompatible device types, including legacy equipment.
In addition, to ensure reliable operation, filters are required to protect data communications from electrical noise and transients. All of these components should meet IP65, IP67, and IP68 environmental standards for operation in industrial settings, and the solution needs to be easy and cost-effective to implement.
This article briefly discusses the problems of connecting legacy equipment to the IIoT. It then introduces the architecture of the Snap Signal family of hardware and software tools from Banner Engineering and how it addresses those challenges. It presents examples of Snap Signal devices including the DXMR90 controller, associated converters, adapters and filters, as well as application considerations when implementing wired and wireless edge computing or cloud connectivity.
Connecting legacy equipment to the IIoT
Many factories predate the appearance of the IIoT and Industry 4.0, and it’s often not possible to interconnect all of the equipment and machines into a single network, resulting in islands of automation. Even if not isolated on an ‘island,’ legacy equipment can be difficult to interconnect as a result of inflexibility arising from the use of proprietary communication protocols, non-standard connectors and cabling, and other factors.
A Snap Signal IIoT overlay network can provide a quick, flexible, and cost-effective way to connect legacy equipment and islands of automation by capturing and converting various non-compatible data communications protocols into an easy to distribute standard, able to be delivered to edge or cloud compute resources for analysis and action (Figure 1).
Figure 1: A Snap Signal overlay network provides a modular architecture to connect legacy equipment and islands of automation with edge or cloud computing resources. (Image source: Banner Engineering)
There are several key components needed to deploy flexible and reliable IIoT overlay networks:
- Adapters to reroute wiring and link various equipment wiring schemes from sensors, indicators and other devices to a standard format used in the overlay network.
- Data converters to translate incompatible formats such as discrete, analog, and various digital formats found on legacy equipment or automation islands into standard protocols such as IO-Link or Modbus to enable centralized performance monitoring.
- Filters to protect the data from corruption in electrically noisy industrial environments, improving signal integrity and reliability and reducing troubleshooting requirements.
- A programmable controller to consolidate data from multiple sources and provide local data processing, as well as connectivity enabling legacy equipment and islands of automation to be integrated into the IIoT.
- A wired or wireless connection to distribute the collected data to edge computing resources and/or the cloud such as Banner’s Cloud Data Service (CDS), which provides data visualization and insights into machine performance and to send email or text alerts to support machine operation, maintenance, and repairs in real-time (Figure 2).
Figure 2: Consolidated data can be transmitted with a wired or wireless connection to edge computing resources or to the cloud such as Banner’s CDS (screenshot above). (Image source: Banner Engineering)
Controller for consolidating multiple data streams
The programmable controller and data converters are key elements in designing an overlay network. The DXMR90 industrial controller from Banner serves as the central communications hub that combines signals from multiple Modbus ports into a unified data stream that is forwarded using industrial Ethernet protocols. For example, the model DXMR90-X1 includes four Modbus masters and supports concurrent communication with up to four serial networks (Figure 3).
Figure 3: Ports on the DXMR90 include a configurable Modbus port 0 (on the left side), Modbus master ports (1 to 4 on the bottom), configurable Modbus port 0/PW for RS-485 and incoming power (top right), and a D-coded Ethernet port (bottom right). (Image source: Banner Engineering)
The DXMR90 is a highly integrated communications controller that features:
- The ability to work with a range of Modbus devices, converting Modbus RTU to Modbus TCP/IP, Ethernet I/P, or Profinet.
- Four independent Modbus master ports that can connect slave devices without manually assigning an address to the devices.
- Local control and connectivity with:
- Modbus/TCP, Modbus RTU, Ethernet/IP, and Profinet, automation protocols
- Internet protocols including RESTful API and MQTT with web services from AWS, and others
- Direct email alerts
- Internal logic controller with pre-defined action rules, that is also programmable using MicroPython or ScriptBasic.
- IP65, IP67, and IP68 rated housing simplifies deployment in industrial settings.
- Quick status indications with user-programmable LEDs.
- Wired Ethernet cable or a cellular-enabled DXM controller can be used for connection to databases such as Banner’s CDS.
Converters connect devices in IIoT networks
Efficient data conversion is needed to blend legacy equipment and islands of automation into an overlay network. For this function, designers can use Banner’s small plug-on S15C series in-line converters to convert condition monitoring and process-sensor data from a variety of formats into digital IO-Link data (Figure 4). For example, the S15C-MGN-KQ is a Modbus master to IO-Link device converter that is user-configurable to read up to 60 registers and write up to 15, with predefined Modbus registers automatically sent over IO-Link.
Figure 4: The S15C series in-line data converters can convert various types of signals including discrete, analog, and others to industrial protocols like Modbus, IO-Link, PWM and PFM. (Image source: Banner Engineering)
S15C converters measure 15 millimeters (mm) in diameter with an over-molded IP68 housing and M12 connectivity, and they use the same power supply as the connected device. Use of S15C converters eliminates the 20-meter (m) IO-Link communication limitation since they can be installed at the end of a Modbus link, near the IO-Link master.
The S15C line of converters includes eight models:
- Six Modbus to IO-Link converters for use with Banner’s line of Modbus sensors, including ultrasonic, measuring light curtain, temperature/humidity, vibration/temperature, and GPS. Plus, there is a generic converter that can be configured to enable most Modbus devices to be deployed as IO-Link devices.
- Two analog sensor models that convert 0 to 10 volts DC or 4 to 20 milliampere (mA) signals to their digital values and forward them as IO-Link data.
Wiring adapters and filters complete the network
In addition to a controller and data converters, designers need wiring adapters and noise filters to quickly deploy flexible and cost-effective overlay networks. In-line wiring adapters, such as Banner’s S15A-F14325-M14325-Q, connect directly to a sensor, indicator, or other device to redirect wiring and isolate signals as needed to match specific application needs (Figure 5). These wiring adapters are available in standard and custom configurations.
Figure 5: S15A adapters such as the S15A-F14325-M14325-Q use an M12 connection for easy installation and can reroute wiring as needed to match specific application requirements. (Image source: Banner Engineering)
S15F in-line filters like the S15F-L-4000-Q are also important elements in an overlay network (Figure 6). They can easily solve challenges with electrical noise and transient voltages that can negatively affect network performance. Like the S15A adapters and S15C converters, these filters have M12 connections and are packaged in an over-molded configuration that meets IP65, IP67, and IP68 standards. Installation of an S15F in-line filter can result in improved signal integrity and less need for network troubleshooting.
Figure 6: S15F in-line filters like the S15F-L-4000-Q can be readily used to protect devices from electrical noise and transients, and their M12 connection makes for easy installation wherever needed in the network. (Image source: Banner Engineering)
Snap signal network design and deployment
The design and deployment of a Snap Signal overlay network begins with the identification of the data sources to be monitored. It then needs to be determined if any new sensors or indicators should be added to supplement existing devices. Steps in the design of a Snap Signal network include:
- Using Banner’s system diagram approach to identify and select the Snap Signal components needed for a specific installation.
- Plan the optimal wiring path, including the placement of T-connectors and filters between the devices to be monitored and the DXMR90 controller.
- Determine if the installation will require the use of a wired Ethernet connection for local data consumption or the use of an edge gateway device to wirelessly connect to a cloud platform.
Snap Signal is a true overlay network and does not require the replacement of any existing hardware. The modular plug-and-play Snap Signal architecture makes installation easy:
- Install any new sensors or other devices and add splitter cables to every device to be monitored to maintain the existing connection with machine controls, while also providing a second path onto the overlay network.
- Install the appropriate in-line signal converters.
- Add T-connectors, filters and other network wiring as needed to complete the network and connect to the DXMR90 controller.
- Program the DXMR90 to create custom sensing and control sequences using ScriptBasic or MicroPython programming and/or the embedded action rules.
- Connect the DXMR90 to edge computing resources using the Ethernet connection, or for cloud connections, a cellular-enabled DXM controller.
Conclusion
Overlay IIoT networks can support designers needs to connect legacy equipment and islands of automation into industrial networks enabling the collection of actionable data to support increased productivity across existing factories. The design and implementation of such an overlay network is complex, but as shown, it can be greatly simplified using Banner Engineering’s topology and Snap Signal line. The line includes the DXMR90 industrial controller, data converters, wiring adapters, filters and other elements needed to implement an IIoT overlay network and distribute it to edge computing resources or to the cloud. The programmable, modular, and flexible design of the Snap Signal network architecture supports the addition of new devices and future proofs the installation.
Recommended Reading

Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of DigiKey or official policies of DigiKey.