Laser Level Instr Manual Datasheet by Klein Tools, Inc.
View All Related Products | Download PDF Datasheet
INSTRUCTION MANUAL
FRANÇAIS pg. 17
ESPAÑOL pg. 9
93LCL
Self-Leveling
Cross Line Laser Level
93LCLS
Self-Leveling
Cross Line Laser Level
with Plumb Spot
ENGLISH
Cross Line Laser Level
93LCLS
Self-Leveling
• HORIZONTAL
AND VERTICAL
CROSS LINES
• PLUMB SPOT
(MODEL 93LCLS)
93LCL
93LCLS

2 3
GENERAL SPECIFICATIONS
Klein Tools 93LCL and 93LCLS are self-leveling laser alignment instruments that
can be used to deliver horizontal and/or vertical cross lines for alignment and layout
applications. Furthermore, model 93LCLS can also deliver a plumb spot directly above
the instrument.
• Operating Altitude: 6562 ft. (2000 m)
• Relative Humidity: <80% non-condensing
• Operating Temp: 20°F to 115°F (-10°C to 45°C)
• Storage Temp: -5°F to 140°F (-20°C to 60°C)
• Laser: 630-680nm, ≤1mW each beam, Class II Laser Product
• Accuracy: ±3/32" per 33' (±2mm per 10 m) (Vertical & Horizontal Beams)
• Battery Type: 3 x 1.5V AA Alkaline
• Dimensions: 5.3" x 5.0" x 2.8" (134 x 127 x 65 mm)
• Weight: 26 oz. (820 g) without batteries (model 93LCLS)
• Calibration: Accurate for one year
• Standards: Conforms to: EN61326-1:2013, EN60825-1:2014.
Complies with: 21 CFR 1040.10 and 1040.11 except for deviations
pursuant to laser notice No. 50, dated June 24, 2007.
• Pollution degree: 2
• Ingress Protection: IP54 Dust & Water Resistant
• Electromagnetic Environment: IEC EN61326-1:2013. This equipment meets
requirements for use in basic and controlled electromagnetic environments like
residential properties, business premises, and light-industrial locations.
Specifications subject to change.
WARNINGS
To ensure safe operation and service of the instrument, follow these instructions.
Failure to observe these warnings can result in serious personal injury, fire, or
electrical shock. Retain these instructions for future reference.
WARNING: LASER RADIATION. DO NOT STARE INTO BEAM. Class II Laser.
• Exposing eyes to laser radiation can result in severe and permanent eye injuries.
NEVER look directly into the laser beam emitted by this instrument.
• Do not use the instrument if it appears to be damaged.
• Do not modify the instrument in any way, as to do so could result in emission of
hazardous laser radiation than could result in severe eye injuries .
• Do not use optical equipment such as lenses, prisms, optical scopes, etc. to
transmit, retransmit, or view the laser beam as this could result in severe eye
injuries.
• This product should not be used by untrained operators or operators who have
not read and fully understood the instructions.
• This product should not be used in any location that could result in somebody
looking at or having their eyes inadvertently irradiated by the laser beam as this
could result in severe eye injuries.
• The instrument should be powered off following use to minimize the risks of
inadvertently exposure to hazardous laser radiation that could result in severe eye
injuries.
• Do not remove warning labels from this instrument as this could result in serious
personal injury and increases the risk of exposure to hazardous laser irradiation.
• The instrument should be securely located in a tidy work environment prior to
operation as unexpected drops or movement of the instrument may result in
damage to the instrument and increases the risk of inadvertent exposure to laser
radiation that could result in severe eye injuries.
• This instrument is IP54 dust & water resistant. Following any contact with water,
thoroughly dry the instrument with a dry, lint-free cloth.
• There are no user serviceable parts in this instrument.
ENGLISH

4 5
7. Pendulum with Lasers
8. Horizontal Line Apeture
9. Vertical Line Apeture
10. Plum Spot Apeture (
93LCLS
)
1. Horizontal Line On/Off Button 11. Battery Compartment Door
2. Vertical Line On/Off Button 12. 1/4-20 Tripod Mount
3. Plum Spot On/Off Button (
93LCLS
)13. 5/8-11 Survey Tripod Mount
4. Low Battery Indicator 14. Magnetic Mount Bracket
5. Excessive Tilt Indicator 15. Magnets
6.
Power/Pendulum Lock/Unlock Switch
16. Clamp-On Wall Adapter
FEATURE DETAILS
NOTE: There are no user-serviceable parts inside this instrument.
SYMBOLS ON INSTRUMENT
Vertical
Laser Line
Low Battery
Indicator
Ingress Protection IP54 Rating –
Dust & Water Resistant
Horizontal
Laser Line
Excessive
Tilt Indicator
Hazardous laser radiation, DO NOT
stare into beam or view directly
with optical instruments
Plumb Spot
Laser
Battery
Polarity Warning or Caution
OPERATING INSTRUCTIONS
TURNING LASER BEAMS ON/OFF
Push the ON/OFF buttons for the horizontal line
1
, vertical line
2
, and plumb
spot
3
(93LCLS model only) to turn ON and OFF their respective laser lines. These
buttons are only active once the Pendulum Lock/Unlock Slider Switch
6
has
been set to the Unlocked position. If the Pendulum Slider Switch is moved from the
Unlocked to the Locked position while the laser beams are active, they will be turned
OFF. The different laser lines can be operated independently or simultaneously.
NOTE: The plumb spot application projects laser beams both in upward and downward
directions. The downward beam may be used to locate a specific point on a floor
layout while the upward beam projects that same point to a ceiling.
PENDULUM SLIDER SWITCH & SELF-LEVELING
The laser assemblies are mounted on a pendulum so that the instrument can self-level.
The Pendulum Slider Switch
6
must be in the unlocked position for the instrument
to self-level. If the instrument is tilted by >4° from the horizontal plane, the pendulum
will not be capable of self-leveling; the active laser beams will flash and the Excessive
Tilt Indicator
5
will blink to indicate that the instrument is not level and cannot
self-level. The instrument must be repositioned on a more level geometry for the self-
Leveling pendulum to function appropriately.
Horizontal Laser Line Vertical Laser Line Plumb Laser Line
NOTE: If the instrument indicates that it is not
level (via flashing beams and/or a blinking
Excessive Tilt indicator
5
),
then it should not
be used for laying out level or plumb lines.
NOTE: Following use, the active laser beams
must be turned OFF and the Pendulum Slider
Switch must be placed in the Locked position
prior to storage.
16
2
6
7
8
5
10
31
9
4
TOP
11
SIDE
BACK
1213
BOTTOM
14
Instrument Tilted Excessively
15
ENGLISH

6 7
OPERATING INSTRUCTIONS
MAGNETIC MOUNTING BRACKET 14
The instrument is attached to a magnetic mounting bracket. The bracket may be
magnetically attached to any magnetic structure such as steel studs, ducts, structural
beams, and steel doors. The bracket also features a key-hole for mounting the
instrument using a screw or nail to non-magnetic structures. Once mounted to a
structure via the mounting bracket the instrument can be rotated on the bracket
through 360° to direct the laser beams.
CLAMP-ON WALL ADAPTER 16
The clamp-on wall adapter may be clamped to a structural beam, or wall bracket for
suspended ceiling installations, to present a steel surface onto which the instrument's
magnetic mounting bracket may be attached. Once magnetically attached the
instrument may be positioned to deliver the laser line at the required location. The
clamp-on adapter also features a key-hole for mounting the instrument using a screw
or nail.
Mounted via keyholeMounted via magnet
Adapter mounted on ceiling bracket Adapter mounted via keyhole
CLEANING
Be sure meter is turned off and wipe with a clean, dry lint-free cloth.
Do not
use abrasive cleaners or solvents.
STORAGE
Remove the batteries when the instrument is not in use for a prolonged period of
time. Do not expose to high temperatures or humidity. After a period of storage in
extreme conditions exceeding the limits mentioned in the General Specifications
section, allow the meter to return to normal operating conditions before using.
WARRANTY
www.kleintools.com/warranty
DISPOSAL / RECYCLE
Do not place equipment and its accessories in the trash. Items must be properly
disposed of in accordance with local regulations. Please see www.epa.gov or
www.erecycle.org for additional information.
CUSTOMER SERVICE
KLEIN TOOLS, INC.
450 Bond Street Lincolnshire, IL 60069
1-877-775-5346
customerservice@kleintools.com
www.kleintools.com
MAINTENANCE
BATTERY REPLACEMENT
When the Low Battery indicator
4
is
displayed, the batteries must be replaced.
1. Open the battery compartment door
11
.
2. Remove and recycle three spent AA batteries.
3. Install new batteries (note proper polarity).
4. Close battery compartment,
ensuring that it is securely shut.
ENGLISH

8 9
NOTES
MANUAL DE INSTRUCCIONES
93LCL
Nivel láser autonivelante
de líneas en cruz
93LCL
Nivel láser autonivelante
de líneas en cruz y punto
de plomada
ESPAÑOL
de líneas en cruz
93LCL
Nivel láser autonivelante
• LÍNEAS HORIZONTAL Y
VERTICAL EN CRUZ
• PUNTO DE PLOMADA
(MODELO 93LCLS)
93LCL
93LCLS
ENGLISH

10 11
ADVERTENCIAS
Para garantizar el funcionamiento y servicio seguros del instrumento, siga estas
instrucciones. El incumplimiento de estas advertencias puede provocar lesiones graves,
incendio o descargas eléctricas. Guarde estas instrucciones para consultarlas en el futuro.
A
DVERTENCIA: RADIACIÓN LÁSER. NO MIRAR EL HAZ DE LUZ. Láser Clase II.
• Exponer la vista a la radiación láser puede provocar lesiones oculares graves e
irreversibles. NUNCA mire directamente el haz de láser que emite el instrumento.
• No utilice el instrumento si en apariencia está dañado.
• No modifique el producto de ninguna manera, ya que esto puede provocar la
emisión de radiación láser peligrosa que, a su vez, puede ocasionar lesiones
oculares graves.
• No utilice equipos ópticos como lentes, prismas, telescopios ópticos, etc. para
transmitir, retransmitir o ver el haz del láser, dado que esto puede ocasionar
lesiones oculares graves.
• No deben usar este producto operadores sin capacitación o que no hayan leído y
comprendido completamente las instrucciones.
• Este producto no se debe utilizar en sitios donde alguien pueda mirar el haz o donde
los ojos queden expuestos accidentalmente a la radiación del haz, dado que esto
puede ocasionar lesiones oculares graves.
• Apague el instrumento después de utilizarlo para minimizar los riesgos de una exposición
accidental a la radiación láser peligrosa que podría provocar lesiones oculares graves.
• No quite las etiquetas de advertencia del instrumento ya que esto puede dar lugar a
lesiones graves y aumentar el riesgo de exposición a radiación láser peligrosa.
• Antes de poner en funcionamiento el instrumento, se lo debe ubicar de modo seguro
en un ambiente de trabajo ordenado. Las caídas inesperadas o el movimiento
del instrumento pueden dañar el equipo y aumentar el riesgo de una exposición
accidental a la radiación láser, que a su vez provocará lesiones oculares graves.
• El instrumento tiene una carcasa IP54 resistente al agua y al polvo. Después del
contacto con agua, seque cuidadosamente el instrumento con un paño limpio y
seco que no deje pelusas.
• Este producto no incluye piezas que el usuario pueda reparar.
ESPECIFICACIONES GENERALES
Los instrumentos de alineación láser autonivelantes Klein Tools 93LCL y 93LCLS
proyectan líneas horizontales o verticales en cruz y son útiles para aplicaciones
de posición de elementos y alineación. Además, el modelo 93LCLS también
proporciona un punto de plomada directamente desde la parte superior del
instrumento.
• Altitud de funcionamiento: 6562pies (2000m)
• Humedad relativa: <80 % sin condensación
• Temperatura de operación: 20 °F a 115 °F (-10 °C a 45 °C)
• Temperatura de almacenamiento: -5 °F a 140 °F (-20 °C a 60 °C)
• Láser: 630nm-680nm, ≤1mW por haz, producto con láser Clase II
• Precisión: ±3/32" cada 33' (±2mm cada 10m) (haz vertical y haz horizontal)
• Tipo de batería: 3 alcalinas AA de 1,5V
• Dimensiones: 5,3" × 5,0" × 2,8" (134mm × 127mm × 65mm)
• Peso: 26oz (820g) sin baterías (modelo 93LCLS)
• Calibración: precisa durante un año
• Normas: Cumple con: EN61326-1:2013, EN60825-1:2014.
Satisface: 21 CFR 1040.10 y 1040.11, excepto en lo referente a los
desvíos, de conformidad con el Aviso sobre láser N.º 50, con fecha del
24 de junio de 2007.
• Grado de contaminación: 2
• Protección contra el ingreso de objetos sólidos y líquidos: IP54 resistente al
agua y al polvo
• Entorno electromagnético: IEC EN61326-1:2013. Este equipo cumple con los
requisitos apropiados para su uso en entornos electromagnéticos básicos y
controlados como propiedades residenciales, establecimientos comerciales e
instalaciones de industria ligera.
Especificaciones sujetas a cambios.
ESPAÑOL

12 13
INSTRUCCIONES DE OPERACIÓN
APAGADO/ENCENDIDO DE LOS HACES DEL LÁSER
Presione los botones de Encendido/Apagado para encender y apagar la línea horizontal
1
, la línea
vertical
2
y el punto de plomada
3
(solo modelo 93LCLS), respectivamente. Estos botones
solo están activos una vez que el interruptor deslizante para bloquear y desbloquear el péndulo
6
se coloca en la posición de desbloqueado. Si se mueve el interruptor de la posición de desbloqueado
a la posición de bloqueado mientras los haces del láser están activos, estos se apagarán. Las
diferentes líneas del láser pueden funcionar independientemente o en forma simultánea.
NOTA: La aplicación de punto de plomada proyecta los haces del láser en dirección
hacia arriba y hacia abajo. El haz hacia abajo se puede utilizar para ubicar un punto
específico en el piso mientras el haz hacia arriba proyecta ese mismo punto en el techo.
INTERRUPTOR DESLIZANTE DEL PÉNDULO Y AUTONIVELACIÓN
Los conjuntos láser están montados sobre un péndulo para que el instrumento pueda
autonivelarse. El interruptor deslizante del péndulo
6
debe estar en la posición de
desbloqueo para que el instrumento se autonivele. Si se inclina el instrumento un ángulo de
más de 4° respecto del plano horizontal, el péndulo no podrá autonivelarse. Los haces del
láser activos se encenderán en forma intermitente y el indicador de inclinación excesiva
5
parpadeará para señalar que el instrumento no está nivelado y que no puede autonivelarse.
Deberá reposicionar el instrumento en una geometría más nivelada para que el péndulo de
autonivelación funcione correctamente.
Línea láser horizontal Línea láser vertical
Línea láser de plomada
7. Péndulo con láseres
8. Apertura de la línea horizontal
9. Apertura de la línea vertical
10. Apertura del punto de
plomada (93LCLS)
1. Botón de encendido/apagado de la 11. Tapa del compartimento de baterías
línea horizontal 12. Orificio de montaje para
2. Botón de encendido/apagado de la línea vertical trípode, 1/4-20
3. Botón de encendido/apagado del punto 13. Orificio de montaje para trípode
de plomada (
93LCLS
) topográfico, 5/8-11
4. Indicador de batería baja 14. Soporte magnético
5. Indicador de inclinación excesiva 15. Imanes
6.
Interruptor de bloqueo/desbloqueo
del péndulo y de encendido
16. Adaptador para sujeción
sobre pared
DETALLES DE LAS CARACTERÍSTICAS
NOTA: Este producto no contiene en su interior piezas que el usuario pueda reparar.
SÍMBOLOS EN EL INSTRUMENTO
Línea
láser vertical
Indicador de
batería baja
Clasificación IP54 de protección contra
el ingreso de objetos sólidos y líquidos:
resistente al agua y al polvo
Línea láser
horizontal
Indicador de
inclinación excesiva
Radiación láser peligrosa, NO mirar el
haz de luz ni mirar directamente
con instrumentos ópticos
Láser de punto de
plomada
Polaridad de la
batería Advertencia o precaución
16
2
6
7
8
5
10
31
9
4
VISTA SUPERIOR
11
VISTA TRASERA VISTA LATERAL
1213
VISTA INFERIOR
15
NOTA: Si el instrumento indica que no está nivelado
(los haces del láser se encienden de manera
intermitente o el indicador de inclinación excesiva
5
parpadea),
no se lo debe utilizar para nivelación
de posición de elementos o líneas de plomada.
NOTA: Después del uso y antes de guardar el
instrumento, los haces activos del láser se deben
APAGAR y el interruptor deslizante del péndulo se
debe colocar en la posición de bloqueado.
Inclinación excesiva
del instrumento
14
ESPAÑOL

14 15
INSTRUCCIONES DE OPERACIÓN
SOPORTE MAGNÉTICO
14
El instrumento está acoplado a un soporte magnético. Este soporte se puede fijar
magnéticamente a cualquier estructura magnética, como pernos de acero, conductos, perfiles
laminados y puertas de acero. También cuenta con un orificio de montaje que sirve para fijar
el instrumento sobre estructuras no magnéticas utilizando un tornillo o clavo. Una vez que
el instrumento está fijado a una estructura mediante su soporte, se lo puede rotar sobre el
soporte 360° para dirigir los haces del láser en la dirección que se desee.
ADAPTADOR DE SUJECIÓN PARA PARED
16
Este adaptador se puede fijar a un perfil laminado o a un soporte de pared en instalaciones de
cielo raso suspendido de modo tal que quede expuesta la superficie de acero sobre la cual se
acoplará el soporte magnético del instrumento. Una vez que el instrumento queda fijado de
forma magnética, se lo puede posicionar para que proporcione una línea láser en la ubicación
requerida. El adaptador de sujeción para pared también cuenta con un orificio de montaje para
fijar el instrumento utilizando un tornillo o clavo.
Fijado mediante orifi cio de montajeFijado mediante imán
Adaptador montado sobre el
soporte del cielo raso Adaptador montado mediante
orifi cio de montaje
LIMPIEZA
Asegúrese de que el medidor esté apagado y límpielo con un paño limpio, seco, que no
deje pelusas.
No utilice solventes ni limpiadores abrasivos.
ALMACENAMIENTO
Retire las baterías si no va a utilizar el instrumento durante un tiempo prolongado. No lo exponga
a la humedad ni a altas temperaturas. Luego de un período de almacenamiento en condiciones
extremas que sobrepasen los límites mencionados en la sección Especificaciones generales, deje
que el medidor vuelva a las condiciones de funcionamiento normales antes de utilizarlo.
GARANTÍA
www.kleintools.com/warranty
ELIMINACIÓN/RECICLAJE
No arroje el equipo ni sus accesorios a la basura. Los elementos se deben
desechar correctamente de acuerdo con las regulaciones locales. Para obtener más
información, consulte www.epa.gov o www.erecycle.org.
SERVICIO AL CLIENTE
KLEIN TOOLS, INC.
450 Bond Street Lincolnshire, IL 60069
1-877-775-5346
customerservice@kleintools.com
www.kleintools.com
MANTENIMIENTO
REEMPLAZO DE LAS BATERÍAS
Cuando aparece el indicador de batería baja
4
, se
deben reemplazar las baterías.
1. Abra la puerta del compartimento de baterías
11
.
2. Retire y envíe las tres baterías AA agotadas
a reciclaje.
3. Instale baterías nuevas (tenga en cuenta la
polaridad correcta).
4. Cierre el compartimento de baterías y asegúrese
de que esté correctamente cerrado.
ESPAÑOL

16 17
NOTAS
MANUEL D’UTILISATION
93LCL
Niveau laser en croix
à nivellement automatique
93LCLS
Niveau laser
en croix à nivellement
automatique à plomb
FRANÇAIS
à nivellement automatique
93LCLS
Niveau laser
• LIGNES
HORIZONTALES
ET VERTICALES
EN CROIX
• PLOMB
(MODÈLE93LCLS)
93LCL
93LCLS
ESPAÑOL

18 19
AVERTISSEMENTS
Pour garantir une utilisation et un entretien sécuritaires de votre instrument, suivez ces
consignes. Le non-respect de ces avertissements peut entraîner de sérieux risques de
blessures, d’incendie ou de choc électrique. Conservez ces instructions à des fins de référence.
AVERTISSEMENT: RADIATION LASER. NE REGARDEZ PAS DIRECTEMENT LE
FAISCEAU. Laser de classeII.
• Faire entrer la radiation laser en contact avec l’œil peut causer des blessures graves et
permanentes aux yeux. Ne regardez JAMAIS directement le faisceau laser émis par cet
instrument.
• N’utilisez pas cet instrument s’il semble endommagé.
• Ne modifiez l’instrument d’aucune façon. Autrement, vous risquez de lancer l’émission de
radiations laser dangereuses provoquant de sérieuses blessures aux yeux.
• N’utilisez pas de matériel optique tel que des lentilles, des prismes ou même des jumelles
dans le but de transmettre, retransmettre ou visionner le faisceau laser; vous pourriez
subir de sérieuses blessures aux yeux.
• Ce produit ne devrait être utilisé que par des opérateurs qualifiés ou par ceux ayant bien
lu et comprit les directives.
• Ce produit ne devrait pas être utilisé dans un emplacement où quelqu’un pourrait
regarder dans l’instrument par accident ou encore où les faisceaux laser peuvent entrer
en contact avec des yeux par inadvertance. Dans les deuxcas, cela pourrait provoquer
des blessures sérieuses aux yeux.
• Après utilisation, l’instrument devrait être éteint pour éliminer les risques d’exposition aux
radiations laser dangereuses pouvant causer de graves blessures aux yeux.
• Ne retirez pas les étiquettes de mise en garde sur l’instrument; cela pourrait augmenter le risque
de subir des blessures sérieuses et le risque d’exposition aux radiations laser dangereuses.
• Après utilisation, l’instrument devrait être mis en lieu sûr dans un environnement propre.
Cela protège l’instrument des chutes et des mouvements accidentels, ces éléments pouvant
endommager l’instrument et donc augmenter les risques d’exposition aux radiations laser
dangereuses pouvant causer de graves blessures aux yeux.
• Cet instrument est conforme à la normeIP54 en ce qui concerne la résistance à l’eau et à la
poussière. En cas de contact avec l’eau, séchez l’instrument avec un linge sec et non pelucheux.
• Cet instrument ne contient aucune pièce réparable par l’utilisateur.
CARACTÉRISTIQUES GÉNÉRALES
Les niveaux KleinTools93LCL et 93LCLS sont des instruments d’alignement laser à
nivellement automatique servant à projeter des croix formées d’une ligne horizontale
et d’une ligne verticale, et ce, à des fins de mise en place et d’alignement. De plus, la
partie supérieure du modèle93LCLS comporte un laser à plomb.
• Altitude de fonctionnement: 2000m (6562pi)
• Humidité relative: <80% (sans condensation)
• Température de fonctionnement: -10°C à 45°C (20°F à 115°F)
• Température d’entreposage: -20°C à 60°C (-5°F à 140°F)
• Laser: 630 à 680nm, ≤1mW pour chaque faisceau, produit laser de classeII
• Précision: ±2mm par 10m (±3/32po par 33pi) (faisceaux à l’horizontal et à
la verticale)
• Type de pile: 3piles alcalineAA 1,5V
• Dimensions: 134x 127x 65mm (5,3x 5,0x 2,8po)
• Poids: 820g (26oz) sans les piles (modèle93LCLS)
• Étalonnage: Précis pendant unan
• Normes: Conforme aux normes: EN61326-1:2013, EN60825-1:2014.
Respecte les normes: 1040.10 et 1040.11 du Titre21 du CFR,
exception faite des déviations conformément au document
«LaserNotice No.50» daté du 24juin2007.
• Niveau de pollution: 2
• Protection contre les infiltrations: Conforme à la normeIP54 en ce qui
concerne la résistance à l’eau et à la poussière.
• Environnement électromagnétique: IEC EN61326-1:2013. Cet équipement
répond aux exigences pour une utilisation dans des environnements
électromagnétiques ordinaires et contrôlés comme les zones résidentielles, les
locaux commerciaux et les sites industriels légers.
Les caractéristiques techniques peuvent faire l’objet de modifications.
FRANÇAIS

20 21
INSTRUCTIONS D’UTILISATION
ALLUMER ET ÉTEINDRE LES FAISCEAUX DU LASER
Appuyez sur les boutons Marche/Arrêt pour la ligne horizontale
1
, la ligne verticale
2
ainsi que le plomb
3
(modèle93LCLS seulement) afin d’allumer et d’éteindre les lignes
laser correspondantes. Vous ne pouvez appuyer sur ces boutons qu’une fois que le système
de verrouillage du pendule
6
est réglé à la position «déverrouillé». Si le système de
verrouillage du pendule passe de la position «déverrouillé» à «verrouillé» pendant que les
faisceaux laser sont allumés, ces derniers s’éteindront automatiquement. Toutes les lignes
laser peuvent fonctionner séparément ou simultanément.
REMARQUE : L’utilisation du point à plomb permet de projeter des rayons laser à la
fois vers le haut et vers le bas. Le rayon pointant vers le bas peut servir à repérer un
point précis au sol pendant que le rayon pointant vers le haut est projeté sur le point
correspondant au plafond.
SYSTÈME DE VERROUILLAGE DU PENDULE ET NIVELLEMENT AUTOMATIQUE
Les lasers sont montés sur un pendule de manière à ce que l’instrument se mette au niveau
automatiquement. Le système de verrouillage du pendule
6
doit être à la position «déverrouillé»
pour que l’instrument se mette automatiquement au niveau. Si l’instrument est incliné à
l’horizontale à un angle >4°, le pendule ne pourra se mettre automatiquement au niveau. Dans ce
cas, les faisceaux laser actifs et l’indicateur d’inclinaison excessive
5
clignoteront pour indiquer
que l’instrument est incliné, et donc qu’il ne peut se mettre au niveau. L’instrument doit donc être
replacé plus au niveau pour que le pendule à nivellement automatique fonctionne efficacement.
Ligne laser horizontale Ligne laser verticale Ligne laser du plomb
7. Pendule avec lasers
8. Ouverture de la ligne horizontale
9. Ouverture de la ligne verticale
10. Ouverture du plomb (
93LCLS
)
1. Bouton Marche/Arrêt de la ligne horizontale 11. Porte du compartiment à pile
2. Bouton Marche/Arrêt de la ligne verticale 12. Support pour trépied à
3. Bouton Marche/Arrêt du plomb (
93LCLS
) connecteur 1/4-20
4. Indicateur de pile faible 13. Support pour trépied
5. Indicateur d’inclinaison excessive d’arpentage 5/8-11
6.
Mise sous tension/verrouillage/
14. Support à fixation aimantée
déverrouillage du pendule
15. Aimants
16. Adaptateur d’applique au mur
CARACTÉRISTIQUES DÉTAILLÉES
REMARQUE: Cet instrument ne renferme aucune pièce réparable par l’utilisateur.
SYMBOLES SUR L’INSTRUMENT:
Ligne laser
verticale Indicateur de
pile faible
Conforme à la normeIP54 pour la
protection contre les infiltrations–
l’eau et la poussière.
Ligne laser
horizontale
Indicateur
d’inclinaison
excessive
Radiations laser dangereuses– NE
regardez PAS directement le faisceau
ni avec des instruments optiques.
Laser à plomb Polarité
des piles Avertissement ou mise en garde
16
2
6
7
8
5
10
31
9
4
DESSUS
11
CÔTÉ
ARRIÈRE
1213
DESSOUS
15
REMARQUE: Si l’instrument indique qu’il n’est pas
au niveau (autrement dit, si les faisceaux laser ou
l’indicateur d’inclinaison excessive clignotent
5
),
il ne devrait pas servir à définir le niveau ou pour
les lignes de plomb.
REMARQUE: Après l’utilisation de l’instrument,
les faisceaux laser actifs doivent être éteints et le
système de verrouillage du pendule doit être
réglé à «verrouillé» avant l’entreposage.
Inclinaison excessive
de l’instrument
14
FRANÇAIS

22 23
INSTRUCTIONS D’UTILISATION
SUPPORT À FIXATION AIMANTÉE
14
L’instrument est fixé à un support à fixation aimantée. Le support peut être fixé à
toute structure magnétique telle que les tenons en acier, les conduits, les poutres
porteuses ou encore les portes en acier. Le support comporte aussi un trou de
serrure afin de fixer l’instrument avec une vis ou un clou sur des structures non
magnétiques. Une fois installé sur une structure avec le support de fixation,
l’instrument peut pivoter sur 360° pour mieux diriger les faisceaux laser.
ADAPTATEUR D’APPLIQUE AU MUR
16
L’adaptateur d’applique au mur peut être fixé sur une poutre porteuse, ou alors sur
un support mural pour plafond suspendu; tant qu’une surface en acier est accessible
pour y installer le support de fixation magnétique de l’instrument. Une fois fixé
grâce à l’aimant, l’instrument peut être positionné pour projeter une ligne laser vers
l’emplacement désiré. L’adaptateur d’applique comporte aussi un trou de serrure
servant à fixer l’instrument avec une vis ou un clou.
Fixé en trou de serrureFixé par l’aimant
Adaptateur fi xé sur un support pour
plafond suspendu Adaptateur fi xé en trou de serrure
NETTOYAGE
Assurez-vous d’éteindre le luxmètre, puis essuyez-le à l’aide d’un linge non
pelucheux propre.
N’utilisez pas de nettoyant abrasif ou de solvant.
RANGEMENT
Retirez les piles lorsque vous prévoyez ne pas utiliser l’appareil pendant une longue
période. N’exposez pas l’appareil à des températures élevées ou à un taux d’humidité
élevé. Après une période de stockage dans des conditions extrêmes (hors des
limites mentionnées dans la section Caractéristiques générales), laissez le luxmètre
revenir à des conditions d’utilisation normales avant de l’utiliser.
GARANTIE
www.kleintools.com/warranty
MISE AU REBUT/RECYCLAGE
Ne mettez pas l’appareil et ses accessoires au rebut. Ces articles doivent
être éliminés conformément aux règlements locaux. Pour de plus amples
renseignements, consultez les sites www.epa.gov ou www.erecycle.org.
SERVICE À LA CLIENTÈLE
KLEIN TOOLS, INC.
450 Bond Street
Lincolnshire, IL 60069
1-877-775-5346
customerservice@kleintools.com
www.kleintools.com
ENTRETIEN
REMPLACEMENT DES PILES
Lorsque l’indicateur de pile faible
4
apparaît,
remplacez les piles.
1. Ouvrez la porte du compartiment à pile
11
.
2. Retirez et recyclez les troispilesAA à plat.
3. Mettez les nouvelles piles en place
(tenez compte de la polarité).
4. Assurez-vous de ferme le compartiment
des piles de façon sécuritaire.
FRANÇAIS

NOTES / NOTAS / REMARQUES
KLEIN TOOLS, INC.
450 Bond Street
Lincolnshire, IL 60069
1-877-775-5346
customerservice@kleintools.com
www.kleintools.com
1390207 Rev. 08/17 D