Bluetooth Remote Control Datasheet by Terasic Inc.

View All Related Products | Download PDF Datasheet
. I‘I I‘I-I'I'I‘I ‘ ‘I I I I I I I‘ h
Bluetooth_Remote_Control
Terasic Inc.
Abstraction
This application note provides details on how to achieve human-computer
interaction (HCI) with Android device and Terasic A-Cute Car via Bluetooth
using a module, Terasic BTS-TMD. The following instructions will help users
easily learn more about UI design on device and the co-design of software and
hardware on Terasic A-Cute Car. This enables users to develop customized
system. Users can get started by scanning the QR code from any Android
device and download Terasic A-Cute Car application.
Reference Design Overview UART LTC2308 VOLTAGE METER PWM Controller ANDROID APPLICATION Demo Setug Rebuild Proiect lmgort Android Proiect Update Demo File
Bluetooth_Remote_Control
Terasic Inc.
1
Content
Reference Design Overview .. 2
UART ...................................... 5
LTC2308 VOLTAGE METER .... 6
PWM Controller .................... 7
ANDROID APPLICATION ......... 8
Demo Setup ........................... 9
Rebuild Project .................... 11
Import Android Project ....... 11
Update Demo File ................ 13
DEO-Nano Board Cyclone IV FPGA AA Baflery x4 Motor Board Motor Driver x2 BTS Module Buzzer Sensor Board IR ReCeIVer Sensor x7
Bluetooth_Remote_Control
Terasic Inc.
2
Reference Design Overview
Figure 1 shows the Terasic A-Cute Car. It consists of three components, DE0-
Nano mainboard, SCD (Smart Car Daughter card), and sensor daughter card
and optional BTS-TMD. The SCD includes a pair of lamps, buzzer, motor driver
DRV8833, IR receiver, ADC chip LT2308, and TMD (Terasic Mini Digital)
expansion header. The sensor daughter card includes seven photo interrupters
used to track dark line(s) on a white background.
Figure 1 Terasic A-Cute Car
Bluetooth_Remote_Control
Terasic Inc.
3
Figure 2 shows the hardware block diagram of Terasic A-Cute car
remotely controlled via Bluetooth. The Android device remote program is
written in C++ and the operation is executed on SDRAM by Nios II processor.
The pair of Lamps is controlled via PIO. The 1K waveform IP generates 1M
frequency to drive the buzzer and the associated GPIO controls the beep
sound. This demo also monitors the battery power left on A-Cute car in real
time from Android device. Users can read the battery voltage via the LTC2308
ADC chip onboard and the data can be transferred to display on the Android
device.
Figure 2 System block diagram of remote control program on
Terasic A-Cute car via Bluetooth
The optional BTS-TMD is connected to the system via TMD0. The data
transmission interface is UART. The movement of A-Cute car is controlled by
the motor through PWM mechanism. Commands can be sent constantly from
Android device to change the direction and speed of A-Cute car instantly. For
more information about the remote control from Android device, please refer
to the following chapters.
c++ Slruclurs Diagram DSVS IP Hardware Circuil Hardware Component
Bluetooth_Remote_Control
Terasic Inc.
4
Figure 3 shows the software block diagram of the demonstration. The
section on the top is C++ Structure Diagram, which interfaces with the QSYS IP
via Altera Avalon Memory-Mapped (AVMM) bus. Both IORD and IOWR are
used to communicate with the QSYS IP.
Figure 3 Software block diagram of remote control program on
Terasic A-Cute car via Bluetooth
The Main. cpp includes the PIO control for LED, KEY, Lamp, Buzzer, and battery
power detection. The battery power detection uses hardware circuit to
convert voltage measured from analog to 12-bit data. Users can read the data
via PIO and send the UART package the BTS-TMD through UART object to
Android device. The CCar object includes two CDcMotor sub-objects which
control the two DC motors on the A-Cute car. The CDcMotor objects control
the PWM IP to control the speed and rotation direction of DC motors.
Bluetooth_Remote_Control
Terasic Inc.
5
UART
When the Bluetooth paring is complete, the A-Cute car will stay in standby
mode and wait for commands. Table 1 shows the command set of all
commands available. The Nios II processor will analyze the command after
receive it through UART object.
Table 1 Command set
Command
Description
ATSP
Speed setting
ATOF
Set the offset value of two motors for turning the direction
ATOFA
Adjust the sensibility of turning the direction
ATSP
Stop the car
ATLON
Turn on the lamps
ATLOFF
Turn off the lamps
ATSPKER
Honk
ATAB
Show battery level
Bluetooth_Remote_Control
Terasic Inc.
6
LTC2308 Voltage Meter
LTC2308 is a low noise, 500Ksps, 8-channel, 12-bit ADC chip. Its last channel is
used to monitor the input power voltage of A-Cute car. The ADC is configured
as single-ended and the output value 0~4095 represents voltage 0~4.095V i.e.
1LSB represents 1mV. Table 2 show the ADC index.
The last channel of the ADC chip can monitor larger range of input voltage by
dividing input voltage connected to the ADC chip. The digitized value must be
multiplied equally back to get the actual input voltage in mV.
In this demonstration, SPI bus is used to communicate between the FPGA and
the LTC2308. The SPI clock of LTC2308 can be 40MHz at maximal. Considering
the reliability of GPIO cable, 20MHz is used in this demonstration. The source
code of LTC2308 IP is located under the M_METERfolder in the system CD.
The register file of the IP is defined below.
Table 2 Read ADC index
The member functions
IORD(CAR_VOLTAGE_DATA_BASE,0) * 4
can report the input power voltage individually.
Register
Index
Description
Read/Write
0
Not use
R
1
Not use
R
2
Not use
R
3
Not use
R
4
Not use
R
5
Not use
R
6
Not use
R
7
12-bit battery voltage level detection
R
Bluetooth_Remote_Control
Terasic Inc.
7
PWM Controller
The PWM controller generates required duty cycle to control the speed of
motor rotation. The source code of this IP is located under the folder
“ip\TERASIC_DC_MOTOR_PWM” in the system CD. The IP is encrypted as a
QSYS compliant IP. The Table 3 show register file of the IP is defined below.
Register
Index
Register
Name
Description
Read/Write
0
TOTAL_DUR
32-bit integer, which represents the tick
number of one PWM cycle.
RW
1
HIGH_DUR
32-bit integer, which represents the tick
number of high level in one PWM cycle
RW
2
CS
Control Register
Bit0: Start bit
1 : Start
0: Stop
Bit1: direction bit
1: forward
0:backward
RW
Table 3 PWM control register table
The CDCMotorC++ class defined in Motor.cpp/h communicates with the PWM
hardware controller. The member function SetSpeed with an input parameter
fSpeed controls the motor speed and direction. The value range of fSpeed
value range -100.0~100.0. The positive and negative values presents forward
rotary and backward rotary, respectively. The values 100 and -100 represents
maximal speed for forward rotary and backward rotary, respectively. The
SetSpeed function translates the input parameter fSpeed to required PMW
parameters for the PWM controller. The translation formula depends on the
input voltage level, which drives the DC motor. The member function
SetInputPower is designed for users to input the current input voltage level.
After setting the motor speed and calling the member function Start, the
motor rotation can get started. Users can stop the motor rotation by calling
the member function Stop. The CCar C++ class defined in Car.cpp/h control the
movement of A-Cute car by controlling the two DC motors on the A-Cute car.
The member function SetSpeed setups car movement speed and direction.
The member function Start is designed to start the car moving and the
member function Stop is designed to stop the car moving.
Bluetooth_Remote_Control
Terasic Inc.
8
Android Application
The development environment for the A-Cute car is Eclipse and the
corresponding software block diagram of Android application is shown in
Figure 4.
Figure 4 Software block diagram of Android application
An object created to interact with users is known as an Activity. It can be
defined as stop, finish, kill, pause, resume, and restart etc. According to the
illustration, there is a .java file and a corresponding UI .xml file in each Activity.
When the application is executed, it starts from Activity(Boot) and enters the
boot screen for about 4 seconds before the object is switched from there to
Activity(SmartCar).
If the A-Cute car is connected to a device such as Android device via Bluetooth,
the Activity(SmartCar) will be paused and the Activity(Bluetooth) will be
executed. After the connection is established, it will switch back to
Activity(SmartCar). The Service(SmartCar) is running at the background of
Android device and cannot be found on the UI. It is responsible for the
transmission of all commands between the A-Cute car and Android device. The
Bluetooth_Remote_Control
Terasic Inc.
9
Service(Battery) sends command to the A-Cute car for battery power
detection in every 3 seconds via Bluetooth.
Demo Setup
The steps to setup the demonstration are:
1. Insert a BTS-TMD module to the TMD header of SCD card, as shown in
Figure 5.
2. Set the power switch of SDC card to OFF position Install four AA batteries
to the battery holder
3. Set the power switch of SDC card to ON position
4. The demonstration will be executed upon power up. If the default code is
erased, please execute test.bat from the folder below to configure the
FPGA on DE0-Nano:
A-Cute Car CD/DE0_NANO_Remote_Car/demo_batch
Prepare for remote function:
Scan the QR code shown in Figure 6 from Android device to install the
SmartCar application.
Launch the SmartCar application installed
Remote control from Android device via Bluetooth, as shown in Figure 7.
Click “connect a Device” on the right-top corner. Search for Bluetooth
device named RNBT-xxx and connect to it. The status of Bluetooth
connection is shown on the top-left corner.
Click the yellow power button located on the right-top corner to ignite
the car. Click the button again will power off the smart car.
The car movement can be controlled in four directions with the G-
sensor on Android device.
Click the LAMP button on the left to turn on/off the lamps.
Click the center area of the wheel to make the beep sound.
There is a scrollbar under the wheel. It is used to adjust the sensitivity
of car turning.
The orange curve bar on the left-bottom corner shows the estimated
car speed.
Bluetoom Toggle Toggle Lamp Power Oil/0W ONO” BeeD Banery ACHVE' vonage EstimaKed Car Speed Turn Senslllvlw
Bluetooth_Remote_Control
Terasic Inc.
10
Figure 5 Insert BTS module
Figure 6 QR-code for A-Cute car Android
application
Figure 7 GUI of Smart Car application on Android device
nan—aw 17m x 720 wmwm rm awn—«u..— ‘ 7.... Mn.- WW m E s» sm_ ->-~ m ”5.5.... mum" hm... ., 5 WM WNW Um, (WW \(n-bhd‘ ‘VNw‘fln‘qn v‘M-hmwwhwm
Bluetooth_Remote_Control
Terasic Inc.
11
Rebuild Project
The project is built in Quartus II v15.1. The source code is located under the
folder:
A-Cut Car System CD/DE0_NANO_Remote_Car
Users can open the Quartus project file DE0_NANO_Remote_CAR.qpf and click
the menu item “ProcessingStart Compilation” to initiate the rebulid process.
When the compilation is complete, an output file named DE0_NANO_Remote
_CAR.sof will be generated under the output_files folder.
The Nios II project is created by Nios II v15.1 Software Build Tools for Eclipse.
The source code is located under the folder:
A-Cut Car System CD/DE0_NANO_Remote_Car/software
Launch Nios II v15.1 Software Build Tools for Eclipse and set the above folder
as workspace. In the Project Explore Window, right click
RemoteCar_bsp[nios_system” and select “NIOS II Generate BSP” to build the
BSP. Right click “RemoteCarand select “Build Project” to generate binary file.
When the rebuild is complete, an output file named RemoteCar.elf will be
generated under the folder:
A-Cut Car CD/DE0_NANO_Remote_Car/software/RemoteCar
Import Android Project
Both Android SDK and Eclipse ADT Plugin must be installed to complete the
installation for this project prior to the development of Android application.
For more settings about the API 17 used in this demo, please refer to
Figure 8
Figure 8 Edit Device
http://developer‘android.com/sdk/installing/installing-adt.html 9.. w WWW. |:I \W.‘ AM,“ WmmmMmMP-I )m. m M mm. Mm \BW )w, mm )W ® [:ij mar—«s w.dwnmmw‘7g‘wmm mum wmummwvmmmww E] M won-«m mw-m m WmumwanuvvaLL Swim...” nmmmm Wm Eudmmwm CD New EE}
Bluetooth_Remote_Control
Terasic Inc.
12
There are many Android SDK versions to be chosen from and the version 4.2.2
(API 17) must be installed. For more details about the installation, please refer
to:
http://developer.android.com/sdk/installing/installing-adt.html
The project folder needs to be imported prior to the start of building the
project. Choose FileImportAndroidExisting Android Code Into
Workspace from the menu, as shown in Figure 9.
Figure 9 Import existing Android code into workspace
Press Next and browse to the project folder under the root directory. Click the
Finish button, as shown in
Figure 10
Figure 10 Import project to finish
n~:- ,xasnvawmmuamsw ~ ~ 7 ~ I...— Mm =w “mm, 4‘ V . we 7.“. _ ramp». “mm .' "v mxnmrgn WM»... rumba, “mm... x. D... e .H calms—4m:- m. Muwm m mm Mum W.“ mum." M...“ mm- , Mum. mm ,
Bluetooth_Remote_Control
Terasic Inc.
13
Update Demo File
Before the demo file can be downloaded to Android device through Eclipse
tool, the Debug mode must be enabled to allow the installation from an
unknown source. The corresponding driver also needs to be installed on the
host PC. Right-click on the project folder and select Run AS -> Android
Application to download the demo file to Android device, as shown in
Figure 11
Figure 11 Update demo file

Products related to this Datasheet

A-CUTE CAR ROBOTIC KITS