Adafruit Data Logger Shield
Created by Bill Earl
Last updated on 2018-11-27 10:56:16 PM UTC

2
4
4
6
6
7
7
8
8
11
11
12
14
17
17
18
18
18
18
18
19
21
21
22
22
25
26
27
28
28
29
29
30
30
32
32
34
34
34
34
35
39
39
Guide Contents
Guide Contents
Overview
Features:
Installing the Headers
Assembly with male headers
Cut the headers to length:
Position the headers:
Position the shield:
And solder!
Assembly with Stacking Headers:
Position the headers:
And solder!
Place the 2x3 female header on to the Arduino/Metro
Shield Overview
SD Card
Real Time Clock
CR1220 12mm Diameter - 3V Lithium Coin Cell Battery
3.3V Power Supply
User LEDs
Prototyping Area
Breakout Pads
Wiring & Config
Which version do I have?
Older Shield Pinouts
Rev B Shield Pinouts
Older Datalogger Shield Leonardo & Mega Library
Using the SD Library with the Mega and Leonardo
cardinfo
Using the Real Time Clock
What is a Real Time Clock?
Battery Backup
CR1220 12mm Diameter - 3V Lithium Coin Cell Battery
Talking to the RTC
First RTC test
Setting the time
Reading the time
Using the SD Card
4GB Blank SD/MicroSD Memory Card
USB MicroSD Card Reader/Writer - microSD / microSDHC / microSDXC
Formatting under Windows/Mac
Get Card Info
Light and Temperature Logger
Introduction
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 2 of 67

40
40
40
41
42
42
42
43
44
44
45
46
48
48
49
50
54
56
56
56
58
59
59
59
59
60
62
62
64
65
65
65
66
67
Build It!
Items you'll need:
The sensors
Wiring it up
Position the sensors
Prepare some jumpers
Install the Jumpers
Make the connections
Add more jumpers for the Sensors
And also for the LEDs
Solder and trim all connections
Prepare the Battery Pack
Use It!
Sensor test
Logging sketch
Plotting with a spreadsheet
Using Gnuplot
Other plotters
Portable logging
Fridge logging
Conclusion!
Code Walkthrough
Introduction
Includes and Defines
Objects and error()
Setup
Main loop
Timestamping
Log sensor data
Downloads
Files
Revision C Schematics & Fabrication Print
Revision B Schematics
Original Version Schematics
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 3 of 67

Overview
Here's a handy Arduino shield: we've had a lot of people looking for a dedicated and well-designed data logging
shield. We worked hard to engineer an inexpensive but well-rounded design. This shield makes it easy to add a 'hard
disk' with gigabytes of storage to your Arduino!
Our latest version of this popular shield has all the features of the popular original, and is "R3" compatible so you can
use it with just about any Arduino or compatible. You can be up and running with it in less than 15 minutes - saving data
to files on any FAT16 or FAT32 formatted SD card, to be read by any plotting, spreadsheet or analysis program. This
tutorial will also show you how to use two free software programs to plot your data. The included RTC (Real Time
Clock) can be used to timestamp all your data with the current time, so that you know precisely what happened when!
The data logger is a reliable, well-rounded and versatile design. It is easily expanded or modified and come well
supported with online documentation and libraries
Features:
SD card interface works with FAT16 or FAT32 formatted cards. Built in 3.3v level shifter circuitry lets you read or
write super fast and prevents damage to your SD card
Real time clock (RTC) keeps the time going even when the Arduino is unplugged. The coin cell battery backup
lasts for years
Included libraries and example code for both SD and RTC mean you can get going quickly
Prototyping area for soldering connectors, circuitry or sensors.
Two configurable indicator LEDs
Onboard 3.3v regulator is both a reliable reference voltage and also reliably runs SD cards that require a lot of
power to run
Uses the "R3 layout" I2C and ICSP/SPI ports so it is compatible with a wide variety of Arduinos and Arduino-
compatibles
With this new version you can use it with:
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 4 of 67

Arduino UNO or ATmega328 compatible - 4 analog channels at 10 bit resolution, 6 if RTC is not used
Arduino Leonardo or ATmega32u4 compatible - 12 analog channels at 10 bit resolution
Arduino Mega or ATmega2560 compatible - 16 analog inputs (10-bit)
Arduino Zero or ATSAMD21 compatible - 6 analog inputs (12-bit)
Arduino Due compatible - 12 analog inputs (12-bit)
Of course you can log anything you like, including digital sensors that have Arduino libraries, serial data, bit timings,
and more!
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 5 of 67

Installing the Headers
The Adafruit Data Logger shield comes tested assembled with all components and SD socket already on it, but you'll
still need need to put headers on so you can plug it into an Arduino
We don't pre-assemble the headers on because there's two options! You can either use plain 0.1" male headers
(included with the shield) or Arduino Shield Stacking headers (http://adafru.it/85). Both options additionally require a
2x3 female header soldered on.
Assembly with male headers
Most people will be happy with assembling he shield with male headers. The nice thing about using these is they don't
add anything to the height of the project, and they make a nice solid connection. However, you won't be able to stack
another shield on top. Trade offs!
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 6 of 67

Cut the headers to length:
Line the header strip up with the holes on the edge of
the shield and cut 4 sections of header strip to fit.
Position the headers:
Insert the header sections - long pins down - into the
female headers on your Arduino/Metro. Additionally
insert the 2x3 female header into the corresponding
pins on the opposite side as the USB.
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 7 of 67

And solder!
Solder each pin to assure good electrical contact. For
tips on soldering, refer to the Adafruit Guide to Excellent
Soldering (https://adafru.it/c6b).
Flip around and solder the other side as well as the 2x3
header
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 9 of 67

Assembly with Stacking Headers:
Stacking headers give your data logger shield extra flexibility. You can combine it with other shields such as the
RGB/LCD Display shield (http://adafru.it/714) to make a compact logging instrument complete with a user interface. You
can also stack it with one or more Proto-Shields (http://adafru.it/51) to add even more prototyping space for interfacing
to sensors.
Stacking headers are installed from the top of the board instead of the bottom, so the procedure is a little different
than for installing simple male headers.
Position the headers:
Insert the headers from the top of the shield, then flip the shield over and place it on a flat surface. Straighten the
headers so that they are vertical.
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 11 of 67

Be sure to insert the headers from the TOP of the shield so that they can be soldered from the BOTTOM.
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 12 of 67

And solder!
Solder each pin for a solid electrical connection.
Tip: Solder one pin from each header section. If any of
them are crooked, simply re-heat the one solder joint
and straighten it by hand. Once all headers are straight,
continue soldering the rest of the pins.
Flip and solder the other side
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 13 of 67

Shield Overview
The datalogger shield has a few things to make it an excellent way to track data. Here's a rough map of th shield:
Our latest version adds power rails for 5V, 3.3V and Ground:
SD Card
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 18 of 67

The big SD card holder can fit any SD/MMC storage up to 32G and and small as 32MB (Anything formatted FAT16 or
FAT32) If you have a MicroSD card, there are low cost adapters which will let you fit these in. SD cards are tougher to
lose than MicroSD, and there's plenty of space for a full size holder.
Simply Push to insert, or Pull to remove the card from this slot
The SD Activity LED is connected to the clock pin, it will blink when data goes over SPI, which can help you detect
when its ok to remove or insert the SD card or power down the Arduino.
The Level Shifter moves all signals from 3.3 or 5V down to 3.3V so you can use this shield with
any
Arduino safely and
not damage cards. Cheaper shields use resistors to level shift, but this doesn't work well at high speed or at all voltage
levels!
Real Time Clock
This is the time-keeping device. It includes the 8-pin chip, the rectangular 32KHz crystal and a battery holder
The battery holder must contain a battery in order for the RTC to keep track of time when power is removed from the
Arduino! Use any CR1220 compatible coin cell
3.3V Power Supply
An on-board 3.3V LDO (low drop-out type) regulator keeps the shield's 3V parts running smoothly. Some old Arduinos
did not have a full 3.3V regulator and writing to an SD card could cause the Arduino to reboot. To maintain
compatibility we just keep it there. There's also a green PWR (Power) good LED to the right
User LEDs
We have two user-configuratble LEDs. Connect a wire from any Arduino pin to L1 or L2 marked pads and pull high to
turn on LED1 or LED2
The reset button to the right of the LEDs, will reset the entire Arduino, handy for when you want to restart the board
Prototyping Area
The big middle section is filled with 0.1" grid prototyping holes so you can customize your shield with sensors or other
circuitry.
The top two and bottom two rows of proto holes are power rails.
CR1220 12mm Diameter - 3V Lithium Coin Cell Battery
$0.95
IN STOCK
ADD TO CART
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 19 of 67

Breakout Pads
We also have some extra breakouts shown above, around the breakout board area.
To the right of the SD card holder:
CD - this is the card detect pad on the SD card. When this is connected to ground, an SD card is inserted. It is
open-drain, use a pullup (either physical resistor or enabled in software)
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 20 of 67

WP - this is the Write Protect pad on the SD card, you can use this to detect if the write-protect tab is on the card
by checking this pin. It is open-drain, use a pullup (either physical resistor or enabled in software)
SQ - this is the optional Squarewave output from the RTC. You have to send the command to turn this on but its a
way of optionally getting a precision squarewave. We use it primarily for testing. The output is open drain so a
pullup (either physical resistor or enabled in software)
3V - this is the 3V out of the regulator. Its a good quality 3.3V reference which you may want to power sensors.
Up to 50mA is available
Near Digital #10
CS - this is the Chip Select pin for the SD card. If you need to cut the trace to pin 10 because it is conflicting, this
pad can be soldered to any digital pin and the software re-uploaded
Near Digital #3 and #4
L2 and L1 - these are optional user-LEDs. Connect to any digital pin, pull high to turn on the corresponding LED.
The LEDs already have 470 ohm resistors in series.
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 21 of 67

Wiring & Config
As of revision B of the Datalogger shield, we've moved away from using digital pins 10, 11, 12, 13 for SPI and A4, A5 for
I2C. We now use the 2x3 ICSP header, which means that you don't need special customized I2C or SPI libraries to use
with Mega or Leonardo or Zero (or any other future type) of Arduino!
Which version do I have?
This is the older Datalogger shield. In particular, note
that the prototyping area is completely full of 0.1"
spaced holes
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 22 of 67

This is the "R3 compatible" Datalogger. Note that it has a
smaller prototyping area and that there is a 2x3 SPI
header spot on the right
Older Shield Pinouts
On the older shields, the pinout was
fixed
to be:
Digital #13 - SPI clock
Digital #12 - SPI MISO
Digital #11 - SPI MOSI
Digital #10 - SD Card chip select (can cut a trace to re-assign)
SDA connected to A4
SCL connected to A5
The RTC (DS1307) I2C logic level was fixed to 5V
Rev B Shield Pinouts
ICSP SCK - SPI clock
ICSP MISO - SPI MISO
ICSP MOSI - SPI MOSI
Digital #10 - SD Card chip select (can cut a trace to re-assign)
SDA
not
connected to A4
SCL
not
connected to A5
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 23 of 67

The RTC (PCF8523) logic level can be 3V or 5V
On an UNO, note that Digital #13 is the same as ICSP SCK, #12 is ICSP MISO, #11 is ICSP MOSI, SDA is tied to A4 and
SCL is A5. However, that is only true on the UNO! Other Arduino's have different connections. Since the shield no
longer makes the assumption it's on an UNO, it is the most cross-compatible shield.
On the bottom of the Rev B shield, you can see that if you have an older Arduino where there is no ICSP 2x3 header,
and no SDA/SCL pins, you can short the solder jumpers closed.
If you are using the shield with a 3.3V logic Arduino, you may want to change the Vio jumper. This is what the 10K
pullups for I2C are pulled up to. Honestly, the pullups are very weak so if you forget, it's not a big deal. But if you can,
cut the small trace between the center pad and 5V and solder the other side so that Vio is connected to 3V
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 24 of 67

© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 25 of 67

Older Datalogger Shield Leonardo & Mega Library
If your shield looks like the above, and has the 2x3 pin header on the right,
skip this page!
If your shield does not have the 2x3 pin header section and you are using a Mega or Leonardo (e.g. not UNO-
compatible) then you can keep reading!
If you are using an Leonardo or Mega with the older datalogging shield, you will have to replace the existing SD card
library to add 'SD card on any pin' support. If you have an Uno/Duemilanove/Diecimila, this is not required. If you have
a rev B shield, this is also not required!
First, find the "core libraries" folder - if you are using Windows or Linux, it will be in the folder that contains the Arduino
executable, look for a libraries folder. Inside you will see an SD folder (inside that will be SD.cpp SD.h etc)
This is ONLY required if you have the older Datalogger shield which does not have the SPI port connection.
This is ONLY required if you are using a Leonardo or Mega with the older Datalogger shield!
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 26 of 67

Ourside the libraries folder, make a new folder called SDbackup. Then drag the SDfolder into SDbackup, this will
'hide' the old SD library without deleting it.
Note that SDBackup must be outside of the libraries folder in order to
effectively 'hide' the SD library.
Now we'll grab the new SD library, visit https://github.com/adafruit/SD (https://adafru.it/aP6) and click theZIP download
button, or click the button below
https://adafru.it/cxl
https://adafru.it/cxl
Uncompress and rename the uncompressed folder SD. Check that the SD folder contains SD.cpp and SD.h
Place the SD library folder your sketchbook libraries folder. You may need to create the libraries subfolder if its your
first library. For more details on how to install libraries, check out our ultra-detailed tutorial at
(https://adafru.it/aYM)http://learn.adafruit.com/adafruit-all-about-arduino-libraries-install-use (https://adafru.it/aYM)
Using the SD Library with the Mega and Leonardo
Because the Mega and Leonardo do not have the same hardware SPI pinout, you need to specify which pins you will
be using for SPI communication with the card. For the data logger shield, these will be pins 10, 11, 12 and 13. Find the
location in your sketch where SD.begin() is called (like this):
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 27 of 67

and change it to add these pin numbers as follows:
cardinfo
The cardinfo sketch uses a lower level library to talk directly to the card, so it calls card.init() instead of SD.begin().
When calling card.init(), you must change the call to specify the SPI pins, as follows:
// see if the card is present and can be initialized:
if (!SD.begin(chipSelect)) {
// see if the card is present and can be initialized:
if (!SD.begin(10, 11, 12, 13)) {
// we'll use the initialization code from the utility libraries
// since we're just testing if the card is working!
while (!card.init(SPI_HALF_SPEED, chipSelect)) {
// we'll use the initialization code from the utility libraries
// since we're just testing if the card is working!
while (!card.init(SPI_HALF_SPEED, 10, 11, 12, 13)) {
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 28 of 67

Using the Real Time Clock
What is a Real Time Clock?
When logging data, it's often really really useful to have timestamps! That way you can take data one minute apart (by
checking the clock) or noting at what time of day the data was logged.
The Arduino does have a built-in timekeeper called millis() and theres also timers built into the chip that can keep track
of longer time periods like minutes or days. So why would you want to have a separate RTC chip? Well, the biggest
reason is that millis() only keeps track of time
since the Arduino was last powered -
that means that when the power is
turned on, the millisecond timer is set back to 0. The Arduino doesnt know its 'Tuesday' or 'March 8th' all it can tell is
'Its been 14,000 milliseconds since I was last turned on'.
OK so what if you wanted to set the time on the Arduino? You'd have to program in the date and time and you could
have it count from that point on. But if it lost power, you'd have to reset the time. Much like very cheap alarm clocks:
every time they lose power they blink 12:00
While this sort of basic timekeeping is OK for some projects, a data-logger will need to have consistent timekeeping
that doesnt reset when the Arduino battery dies or is reprogrammed. Thus, we include a separate RTC! The RTC chip
is a specialized chip that just keeps track of time. It can count leap-years and knows how many days are in a month,
but it doesn't take care of Daylight Savings Time (because it changes from place to place)
This image shows a computer motherboard with a Real Time Clock called the DS1387 (https://adafru.it/aX0). Theres a
lithium battery in there which is why it's so big.
The RTC we'll be using is the
PCF8523 (https://adafru.it/reb)
or the
DS1307
(https://adafru.it/rec).
If you have an Adafruit Datalogger Shield rev B, you will be using the PCF8523 - this RTC is newer and better than
the DS1307. Look on your shield to see if you see PCF8523 written above the chip.
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 29 of 67

If you have an older Datalogger shield, you will be using the DS1307 - there's no text so you'll just need to remember
that if it
doesn't
say PCF8523 it's the DS1307
Battery Backup
As long as it has a coin cell to run it, the RTC will merrily tick along for a long time, even when the Arduino loses
power, or is reprogrammed.
Use any CR1220 3V lithium metal coin cell battery:
CR1220 12mm Diameter - 3V Lithium Coin Cell Battery
$0.95
IN STOCK
ADD TO CART
You MUST have a coin cell installed for the RTC to work, if there is no coin cell, it will act strangely and
possibly hang the Arduino when you try to use it, so ALWAYS make SURE there's a battery installed, even if
it's a dead battery.
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 30 of 67

Talking to the RTC
The RTC is an i2c device, which means it uses 2 wires to to communicate. These two wires are used to set the time
and retrieve it. On the Arduino UNO, these pins are also wired to the Analog 4 and 5 pins. This is a bit annoying since
of course we want to have up to 6 analog inputs to read data and now we've lost two.
For the RTC library, we'll be using a fork of JeeLab's excellent RTC library, which is available on
GitHub (https://adafru.it/c7r). You can do that by visiting the github repo and manually downloading or, easier, just click
this button to download the zip
https://adafru.it/cxm
https://adafru.it/cxm
Rename the uncompressed folder RTClib and check that the RTClib folder contains RTClib.cpp and RTClib.h
Place the RTClib library folder your arduinosketchfolder/libraries/ folder.
You may need to create the libraries subfolder if it's your first library. Restart the IDE.
We also have a great tutorial on Arduino library installation at:
http://learn.adafruit.com/adafruit-all-about-arduino-libraries-install-use
Once done, restart the IDE
First RTC test
The first thing we'll demonstrate is a test sketch that will read the time from the RTC once a second. We'll also show
what happens if you remove the battery and replace it since that causes the RTC to halt. So to start, remove the battery
from the holder while the Arduino is not powered or plugged into USB. Wait 3 seconds and then replace the battery.
This resets the RTC chip. Now load up the matching sketch for your RTC
For the Adafruit Datalogger shield rev B open up Examples->RTClib->pcf8523
For the older Adafruit Dataloggers, use Examples->RTClib->ds1307
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 31 of 67

Upload it to your Arduino with the datalogger shield on!
Now open up the Serial Console and make sure the baud rate is set correctly at 57600 baud you should see the
following:
Whenever the RTC chip loses all power (including the backup battery) it will reset to an earlier date and report the time
as 0:0:0 or similar. The DS1307 won't even count seconds (it's stopped).Whenever you set the time, this will kickstart
the clock ticking.
So, basically, the upshot here is that you should never ever remove the battery once you've set the time. You shouldn't
have to and the battery holder is very snug so unless the board is crushed, the battery won't 'fall out'
If you're having problems make sure you are running the right example! PCF8523 and DS1307 RTC chips are
not identical so they have separate examples!
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 32 of 67

Setting the time
With the same sketch loaded, uncomment the line that starts with RTC.adjust like so:
This line is very cute, what it does is take the Date and Time according the computer you're using (right when you
compile the code) and uses that to program the RTC. If your computer time is not set right you should fix that first. Then
you must press the Upload button to compile and then immediately upload. If you compile and then upload later, the
clock will be off by that amount of time.
Then open up the Serial monitor window to show that the time has been set
From now on, you won't have to ever set the time again: the battery will last 5 or more years
Reading the time
Now that the RTC is merrily ticking away, we'll want to query it for the time. Let's look at the sketch again to see how
this is done
if (! rtc.initialized()) {
Serial.println("RTC is NOT running!");
// following line sets the RTC to the date & time this sketch was compiled
rtc.adjust(DateTime(F(__DATE__), F(__TIME__)));
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 33 of 67

There's pretty much only one way to get the time using the RTClib, which is to call now(), a function that returns a
DateTime object that describes the year, month, day, hour, minute and second when you called now().
There are some RTC libraries that instead have you call something like RTC.year() and RTC.hour() to get the current
year and hour. However, there's one problem where if you happen to ask for the minute right at 3:14:59 just before the
next minute rolls over, and then the second right after the minute rolls over (so at 3:15:00) you'll see the time as 3:14:00
which is a minute off. If you did it the other way around you could get 3:15:59 - so one minute off in the other direction.
Because this is not an especially unlikely occurance - particularly if you're querying the time pretty often - we take a
'snapshot' of the time from the RTC all at once and then we can pull it apart into day() or second() as seen above. It's a
tiny bit more effort but we think its worth it to avoid mistakes!
We can also get a 'timestamp' out of the DateTime object by calling unixtime which counts the number of seconds (not
counting leapseconds) since midnight, January 1st 1970
Since there are 60*60*24 = 86400 seconds in a day, we can easily count days since then as well. This might be useful
when you want to keep track of how much time has passed since the last query, making some math a lot easier (like
checking if it's been 5 minutes later, just see if unixtime() has increased by 300, you dont have to worry about hour
changes)
void loop () {
DateTime now = rtc.now();
Serial.print(now.year(), DEC);
Serial.print('/');
Serial.print(now.month(), DEC);
Serial.print('/');
Serial.print(now.day(), DEC);
Serial.print(" (");
Serial.print(daysOfTheWeek[now.dayOfTheWeek()]);
Serial.print(") ");
Serial.print(now.hour(), DEC);
Serial.print(':');
Serial.print(now.minute(), DEC);
Serial.print(':');
Serial.print(now.second(), DEC);
Serial.println();
Serial.print(" since 2000 = ");
Serial.print(now.unixtime());
Serial.print("s = ");
Serial.print(now.unixtime() / 86400L);
Serial.println("d");
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 34 of 67

Using the SD Card
The other half of the data logger shield is the SD card. The SD card is how we store long term data. While the Arduino
chip has a permanent EEPROM storage, its only a couple hundred bytes - tiny compared to a 2 gig SD card. SD cards
are so cheap and easy to get, its an obvious choice for long term storage so we use them for the shield.
The shield kit doesn't come with an SD card but we carry one in the shop that is guaranteed to
work (https://adafru.it/aIH). Pretty much any SD card should work but be aware that some cheap cards are 'fakes' and
can cause headaches.
You'll also need a way to read and write from the SD card. Sometimes you can use your camera and MP3 player -
when its plugged in you will be able to see it as a disk. Or you may need an SD card reader (http://adafru.it/939). The
shield doesnt have the ability to display the SD card as a 'hard disk' like some MP3 players or games, the Arduino
does not have the hardware for that, so you will need an external reader!
Formatting under Windows/Mac
If you bought an SD card, chances are it's already pre-formatted with a FAT filesystem. However you may have
problems with how the factory formats the card, or if it's an old card it needs to be reformatted. The Arduino SD library
we use supports both FAT16 and FAT32 filesystems. If you have a very small SD card, say 8-32 Megabytes you might
find it is formatted FAT12 which isnt supported. You'll have to reformat these card. Either way, its always good idea to
format the card before using, even if its new! Note that formatting will erase the card so save anything you want first
4GB Blank SD/MicroSD Memory Card
$7.95
OUT OF STOCK
OUT OF STOCK
USB MicroSD Card Reader/Writer - microSD / microSDHC /
microSDXC
$5.95
IN STOCK
ADD TO CART
We strongly recommend you use the official SD card formatter utility - written by the SD association it solves
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 35 of 67

The official SD formatter is available from https://www.sdcard.org/downloads/formatter_4/ (https://adafru.it/cfL)
Download it and run it on your computer, there's also a manual linked from that page for use
https://adafru.it/cfL
https://adafru.it/cfL
Get Card Info
The Arduino SD Card library has a built in example that will help you test the shield and your connections
If you have an older Datalogging shield without the SPI header connection and you are using a Leonardo, Mega
or anything other than an UNO, you'll need to install a special version of the SD library (https://adafru.it/ref)
Open the file CardInfo example sketch in the SD library:
This sketch will not write any data to the card, just tell you if it managed to recognize it, and some information about it.
This can be very useful when trying to figure out whether an SD card is supported. Before trying out a new card,
please try out this sketch!
many problems that come with bad formatting!
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 36 of 67

Go to the beginning of the sketch and make sure that the chipSelect line is correct, for the datalogger shield we 're
using digital pin 10 so change it to 10!
If you have the pre-rev B version of the Datalogger Shield, and you are using a Mega or Leonardo check here for now
to adjust the pin setup (https://adafru.it/ref)
OK, now insert the SD card into the Arduino and upload the sketch
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 37 of 67

Open up the Serial Monitor and type in a character into the text box (& hit send) when prompted. You'll probably get
something like the following:
Its mostly gibberish, but its useful to see the Volume type is FAT16 part as well as the size of the card (about 2 GB
which is what it should be) etc.
If you have a bad card, which seems to happen more with ripoff version of good brands, you might see:
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 38 of 67

The card mostly responded, but the data is all bad. Note that the Product ID is "N/A" and there is no Manufacturer ID
or OEM ID. This card returned some SD errors. Its basically a bad scene, I only keep this card around to use as an
example of a bad card! If you get something like this (where there is a response but its corrupted) you should toss the
card
Finally, try taking out the SD card and running the sketch again, you'll get the following,
It couldn't even initialize the SD card. This can also happen if there's a soldering error or if the card is
really
damaged
If you're having SD card problems, we suggest using the SD formatter mentioned above first to make sure the card is
clean and ready to use!
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 39 of 67

Light and Temperature Logger
Introduction
OK now that we have introduced both the RTC and the SD card and verified that they're working, we can move onto
logging!
We'll use a pretty good & detailed demonstration to show off the capabilities of this most awesome data logging shield:
We'll log both temperature and relative light levels to determine:
1. How much does the temperature in a fridge vary as the compressor turns on and off?
2. Does keeping the door open cause a big temperature drop? How long does it take for it to cool down?
3. Does the light inside
really
turn off when the door is closed?
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 40 of 67

Build It!
Items you'll need:
Arduino (of course!) a Atmega328 type is best (http://adafru.it/50)- we always recommend going with an official
'classic' Arduino such as the Uno.
Adafruit data logger shield (http://adafru.it/1141) - assembled
SD card formatted for FAT (http://adafru.it/102) and tested using our example sketch (https://adafru.it/clN)
CdS photocell (http://adafru.it/161) and a matching 10K pulldown resistor
Temperature sensor with analog out, such as TMP36 (http://adafru.it/165)
Battery pack such as a 6-AA 'brick' and a 2.1mm DC jack. (http://adafru.it/248)
or you can use a 9V clip for a power supply (http://adafru.it/80) but a 9V powered logger will last only a couple
hours so we suggest 6xAA's
Some 22 AWG wire (https://adafru.it/c79), soldering iron, solder (https://adafru.it/doU), etc.
You can get most everything in that list in a discounted pack in the Adafruit shop! (http://adafru.it/249)
The sensors
We'll use two basic sensors to log data, a CdS photocell to track light (http://adafru.it/161) (this will tell us when the door
has been opened) and a semiconductor temperature sensor to log the ambient fridge temperature. (http://adafru.it/165)
We have two great tutorials for these sensors on our site, if you haven't used them before or need some refreshment,
please read them now!
https://adafru.it/reg
https://adafru.it/reg
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 41 of 67

https://adafru.it/reh
https://adafru.it/reh
We will wire the sensors as shown in the diagram below.
Note that we connect ARef, the power pin of the temp sensor, and the light sensor to 3.3V
not to 5.0V
- we do this
because the 5V line is very noisy and the 3.3V regulator is better filtered. In the actual board we used the 3.3V line
from the datalogger's regulator, see the images below - in theory its the same as the one off of the Arduino but we
trust ours more.
Wiring it up
The prototyping area on the board is a simple array of holes with soldering pads. The steps below show how we built
this circuit and illustrate some some basic circuit prototyping techniques. For clarity, we will use the same color wire as
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 42 of 67

shown in the circuit diagram above:
Position the sensors
The sensors could go anywhere on the prototyping
area, but we chose this arrangement to simplify
connections between the components later on.
Prepare some jumpers
Measure a piece of wire (red) long enough to reach from
the 3v breakout hole to 1/2" past the temperature
sensor. Strip about 3/4" from one end, and about 1/4"
from the other.
Measure another one (yellow) long enough to reach
from the AREF pin to the hole between the two sensors.
Strip 1/2" from one end and 1/4" from the other.
Install the Jumpers
Place the jumpers as shown, with the long stripped ends
nearest the sensors.
Since there are no signal traces between the holes in
the prototyping area, we will use the long stripped ends
to join the legs of the components on the board.
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 43 of 67

Make the connections
Solder the first jumper (red) to the 3v hole.
Bend the stripped end of the wire so it rests next
to the legs of the light sensor, the temperature
sensor and the end of the AREF jumper.
Fold the sensor legs and AREF jumper legs over
the 3v jumper and solder to make the connection.
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 44 of 67

Add more jumpers for the Sensors
From Analog Pin 0 to the hole near the light
sensor and resistor. (white)
From GND to the hole next to the other end of the
resistor (black)
From the Analog pin 1 to the hole next to the
center pin of the temperature sensor (green)
And also for the LEDs
From L1 to Digital Pin 2 (yellow)
From L2 to Digital Pin 3 (yellow)
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 45 of 67

Solder and trim all connections
Using the same technique of folding the component
legs over the jumper - make all connections as shown in
the wiring diagram.
Make sure that all connections are soldered. Also solder
wires and component legs to the board where they pass
through the holes.
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 46 of 67

Prepare the Battery Pack
Place the black plastic ferrule from the connector
over the battery pack wires.
Solder the red wire from the battery pack to the
center pin
Solder the the black wire to the outer barrel.
Crimp to hold the wires securely
Screw the black plastic ferrule on to cover the
solder joints.
Now your Light Temp Logger is wired and ready for testing!
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 47 of 67

© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 48 of 67

Use It!
Sensor test
We'll now test the sensors, using this sketch which is a bit of a mashup of the two examples in our
tutorials (https://adafru.it/c7d)
#include <SPI.h>
#include <SD.h>
/* Sensor test sketch
for more information see http://www.ladyada.net/make/logshield/lighttemp.html
*/
#define aref_voltage 3.3 // we tie 3.3V to ARef and measure it with a multimeter!
int photocellPin = 0; // the cell and 10K pulldown are connected to a0
int photocellReading; // the analog reading from the analog resistor divider
//TMP36 Pin Variables
int tempPin = 1; //the analog pin the TMP36's Vout (sense) pin is connected to
//the resolution is 10 mV / degree centigrade with a
//500 mV offset to allow for negative temperatures
int tempReading; // the analog reading from the sensor
void setup(void) {
// We'll send debugging information via the Serial monitor
Serial.begin(9600);
// If you want to set the aref to something other than 5v
analogReference(EXTERNAL);
}
void loop(void) {
photocellReading = analogRead(photocellPin);
Serial.print("Light reading = ");
Serial.print(photocellReading); // the raw analog reading
// We'll have a few threshholds, qualitatively determined
if (photocellReading < 10) {
Serial.println(" - Dark");
} else if (photocellReading < 200) {
Serial.println(" - Dim");
} else if (photocellReading < 500) {
Serial.println(" - Light");
} else if (photocellReading < 800) {
Serial.println(" - Bright");
} else {
Serial.println(" - Very bright");
}
tempReading = analogRead(tempPin);
Serial.print("Temp reading = ");
Serial.print(tempReading); // the raw analog reading
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 49 of 67

OK upload this sketch and check the Serial monitor again
In my workroom, I got about 24 degrees C and a 'light measurement' of about 400 - remember that while the
temperature sensor gives an 'absolute' reading in C or F, the light sensor is not precise and can only really give rough
readings.
Once you've verified that the sensors are wired up correctly & running its time to get to the logging!
Logging sketch
Download the light and temperature logging sketch from GitHub (https://adafru.it/c7e). Insert the SD card.
Look at the top of the sketch for this section and uncomment whichever line is relevant. Check the RTC page for
details if you're not sure which one you have. (https://adafru.it/rei)
// converting that reading to voltage, which is based off the reference voltage
float voltage = tempReading * aref_voltage / 1024;
// print out the voltage
Serial.print(" - ");
Serial.print(voltage); Serial.println(" volts");
// now print out the temperature
float temperatureC = (voltage - 0.5) * 100 ; //converting from 10 mv per degree wit 500 mV offset
//to degrees ((volatge - 500mV) times 100)
Serial.print(temperatureC); Serial.println(" degrees C");
// now convert to Fahrenheight
float temperatureF = (temperatureC * 9 / 5) + 32;
Serial.print(temperatureF); Serial.println(" degrees F");
delay(1000);
}
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 50 of 67

Upload the sketch to your Arduino. We'll now test it out while still 'tethered' to the computer
While the Arduno is still connected, blinking and powered, place your hand over the photocell for a few seconds, then
shine a flashlight on it. You should also squeeze the temp sensor with your fingers to heat it up
Plotting with a spreadsheet
When you're ready to check out the data, unplug the Arduino and put the SD card into your computer's card reader.
You'll see a at least one and perhaps a couple files, one for each time the logger ended up running
We'll open the most recent one. If you want to use the same logfile used in the graphing demos, click here to
download it (https://adafru.it/cny).
The quickest way to look at the data is using something like OpenOffice or Excel, where you can open the .csv file and
have it imported directly into the spreadsheet
/************** if you have a DS1307 uncomment this line **************/
//RTC_DS1307 RTC; // define the Real Time Clock object
/************** if you have a PCF8523 uncomment this line **************/
//RTC_PCF8523 RTC; // define the Real Time Clock object
/**********************************************************************/
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 51 of 67

You can then perform some graphing by selecting the columns of data
Clicking the Chart button and using Lines (we think they are the best for such graphs)
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 52 of 67

Setting the First Column as label
Which will generate this graph
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 53 of 67

You can see pretty clearly how I shaded the sensor and then shone a flashlight on it.
You can make the graph display both with different axes (since the change in temperature is a different set of units.
Select the temp line (red), right-click and choose Format Data Series. In the Options tab, Align data series to
Secondary Y-axis.
Or you can make another graph with only the temp data
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 54 of 67

Now you can see clearly how I warmed up the sensor by holding it between my fingers
Using Gnuplot
Gnuplot is an free (but not open source?), ultra-powerful plotting program. Its also a real pain to use! But if you can't
afford a professional math/plotting package such as Mathematica or Matlab, Gnuplot can do a lot!
We're not good enough to provide a full tutorial on gnuplot, here are a few links we found handy. Google will definitely
help you find even more tutorials and links. Mucking about is the best teacher, too!
http://www.cs.hmc.edu/~vrable/gnuplot/using-gnuplot.html (https://adafru.it/c7i)
http://www.duke.edu/~hpgavin/gnuplot.html (https://adafru.it/c7k)
http://www.ibm.com/developerworks/library/l-gnuplot/ (https://adafru.it/c7m)
We found the following commands executed in order will generate a nice graph of this data, be sure to put
LOGTEST.CSV in the same directory as wgnuplot.exe (or if you know how to reference directories, you can put it
elsewhere)
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 55 of 67

Which makes this:
set xlabel "Time" # set the lower X-axis label to 'time'
set xtics rotate by -270 # have the time-marks on their side
set ylabel "Light level (qualitative)" # set the left Y-axis label
set ytics nomirror # tics only on left side
set y2label "Temperature in Fahrenheit" # set the right Y-axis label
set y2tics border # put tics no right side
set key box top left # legend box
set key box linestyle 0
set xdata time # the x-axis is time
set format x "%H:%M:%S" # display as time
set timefmt "%s" # but read in as 'unix timestamp'
plot "LOGTEST.CSV" using 2:4 with lines title "Light levels"
replot "LOGTEST.CSV" using 2:5 axes x1y2 with lines title "Temperature (F)"
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 56 of 67

Note the cool double-sided y-axis scales! You can zoom in on stuff pretty easily too.
Other plotters
Our friend John also suggests Live-Graph as a free plotting program (https://adafru.it/c7o)
(https://adafru.it/c7o) - we
haven't tried it but its worth looking at if you need to do a lot of plotting!
Portable logging
Of course, having a datalogger thats chained to a desktop computer isn't that handy. We can make a portable logger
with the addition of a battery pack. The cheapest way to get a good amount of power is to use 6 AA batteries. I made
one here with rechargables and a 6xAA battery holder (http://adafru.it/248). It ran the Arduino logging once a second
for 18.5 hours. If you use alkalines you could easily get 24 hours or more.
Fridge logging
With my portable logger ready, its time to do some Fridge Loggin'! Both were placed in the fridge, in the center of the
middle shelf.
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 57 of 67

I placed it in around 10PM and then removed it around noon the next day. If you don't have a fridge handy, you can
grab the data from this zip file and use that (https://adafru.it/cnz).
Here is the logged data:
You can see in the middle and end the temp and light levels are very high because the logger was outside the fridge.
The green line is the temperature so you can see the temperature slowly rising and then the compressor kicking in
every half hour or so. The red lines indicate when the door was opened. This night was a more insominac one than
normal!
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 58 of 67

Zooming into the plot at about 12:40AM, we can see how the temperature climbs whenever the door is open, even in a
few seconds it can climb 4 degrees very quickly!
Conclusion!
OK that was a detailed project but its a good one to test your datalogging abilities, especially since its harder to fix
bugs in the field. In general, we suggest trying other sensors and testing them at home if possible. Its also a good idea
to log more data than you need, and use a software program to filter anything you dont need. For example, we dont
use the VCC log but if you're having strange sensor behavior, it may give you clues if your battery life is affecting it.
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 59 of 67

Code Walkthrough
Introduction
This is a walkthrough of the Light and Temperature Logging sketch. Its long and detailed so we put it here for your
perusal. We strongly suggest reading through it, the code is very versatile and our text descriptions should make it
clear why everything is there!
Download the complete file here (https://adafru.it/c7e):
Includes and Defines
OK this is the top of the file, where we include the three libraries we'll use: the SD library to talk to the card, the Wire
library that helps the Arduino with i2c and the RTClib for chatting with the real time clock
Next are all the "defines" - the constants and tweakables.
LOG_INTERVAL is how many milliseconds between sensor readings. 1000 is 1 second which is not a bad starting
point
ECHO_TO_SERIA L determines whether to send the stuff thats being written to the card also out to the Serial
monitor. This makes the logger a little more sluggish and you may want the serial monitor for other stuff. On the
other hand, its hella useful. We'll set this to 1 to keep it on. Setting it to 0 will turn it off
WAIT_TO_START means that you have to send a character to the Arduino's Serial port to kick start the logging. If
you have this on you basically can't have it run away from the computer so we'll keep it off (set to 0) for now. If
you want to turn it on, set this to 1
The other defines are easier to understand, as they are just pin defines
redLEDpin is whatever you connected to the Red LED on the logger shield
greenLEDpin is whatever you connected to the Green LED on the logger shield
photocellPin is the analog input that the CdS cell is wired to
tempPin is the analog input that the TMP36 is wired to
Objects and error()
#include "SD.h"
#include <Wire.h>
#include "RTClib.h"
// A simple data logger for the Arduino analog pins
#define LOG_INTERVAL 1000 // mills between entries
#define ECHO_TO_SERIAL 1 // echo data to serial port
#define WAIT_TO_START 0 // Wait for serial input in setup()
// the digital pins that connect to the LEDs
#define redLEDpin 3
#define greenLEDpin 4
// The analog pins that connect to the sensors
#define photocellPin 0 // analog 0
#define tempPin 1 // analog 1
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 60 of 67

Next up we've got all the objects for the RTC, and the SD card chip select pin. For all our shields we use pin 10 for SD
card chip select lines
Next is the error() function, which is just a shortcut for us, we use it when something Really Bad happened, like we
couldn't write to the SD card or open it. It prints out the error to the Serial Monitor, turns on the red error LED, and then
sits in a while(1); loop forever, also known as a halt
Setup
K now we are onto the code. We begin by initializing the Serial port at 9600 baud. If we set WAIT_TO_START to
anything but 0, the Arduino will wait until the user types something in. Otherwise it goes ahead to the next part
RTC_DS1307 RTC; // define the Real Time Clock object
// for the data logging shield, we use digital pin 10 for the SD cs line
const int chipSelect = 10;
// the logging file
File logfile;
void error(char *str)
{
Serial.print("error: ");
Serial.println(str);
// red LED indicates error
digitalWrite(redLEDpin, HIGH);
while(1);
}
void setup(void)
{
Serial.begin(9600);
Serial.println();
#if WAIT_TO_START
Serial.println("Type any character to start");
while (!Serial.available());
#endif //WAIT_TO_START
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 61 of 67

Now the code starts to talk to the SD card, it tries to initialize the card and find a FAT16/FAT32 partition.
Next it will try to make a logfile. We do a little tricky thing here, we basically want the files to be called something like
LOGGERnn.csv where nn is a number. By starting out trying to create LOGGER00.CSV and incrementing every time
when the file already exists, until we get to LOGGER99.csv, we basically make a new file every time the Arduino starts
up
To create a file, we use some Unix style command flags which you can see in the logfile.open() procedure. FILE_WRITE
means to create the file and write data to it.
Assuming we managed to create a file successfully, we print out the name to the Serial port.
// initialize the SD card
Serial.print("Initializing SD card...");
// make sure that the default chip select pin is set to
// output, even if you don't use it:
pinMode(10, OUTPUT);
// see if the card is present and can be initialized:
if (!SD.begin(chipSelect)) {
Serial.println("Card failed, or not present");
// don't do anything more:
return;
}
Serial.println("card initialized.");
// create a new file
char filename[] = "LOGGER00.CSV";
for (uint8_t i = 0; i < 100; i++) {
filename[6] = i/10 + '0';
filename[7] = i%10 + '0';
if (! SD.exists(filename)) {
// only open a new file if it doesn't exist
logfile = SD.open(filename, FILE_WRITE);
break; // leave the loop!
}
}
if (! logfile) {
error("couldnt create file");
}
Serial.print("Logging to: ");
Serial.println(filename);
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 62 of 67

OK we're wrapping up here. Now we kick off the RTC by initializing the Wire library and poking the RTC to see if its
alive.
Then we print the header. The header is the first line of the file and helps your spreadsheet or math program identify
whats coming up next. The data is in CSV (comma separated value) format so the header is too: "millis,time,light,temp"
the first item millis is milliseconds since the Arduino started, time is the time and date from the RTC, light is the data
from the CdS cell and temp is the temperature read.
You'll notice that right after each call to logfile.print() we have #if ECHO_TO_SERIAL and a matching Serial.print() call
followed by a #if ECHO_TO_SERIAL this is that debugging output we mentioned earlier. The logfile.print() call is what
writes data to our file on the SD card, it works pretty much the same as the Serial version. If you set ECHO_TO_SERIAL
to be 0 up top, you won't see the written data printed to the Serial terminal.
Finally, we set the two LED pins to be outputs so we can use them to communicate with the user. There is a
commented-out line where we set the analog reference voltage. This code assumes that you will be using the 'default'
reference which is the VCC voltage for the chip - on a classic Arduino this is 5.0V. You can get better precision
sometimes by lowering the reference. However we're going to keep this simple for now! Later on, you may want to
experiment with it.
Main loop
Now we're onto the loop, the loop basically does the following over and over:
1. Wait until its time for the next reading (say once a second - depends on what we defined)
2. Ask for the current time and date froom the RTC
3. Log the time and date to the SD card
4. Read the photocell and temperature sensor
5. Log those readings to the SD card
6. Sync data to the card if its time
Timestamping
Wire.begin();
if (!RTC.begin()) {
logfile.println("RTC failed");
#if ECHO_TO_SERIAL
Serial.println("RTC failed");
#endif //ECHO_TO_SERIAL
}
logfile.println("millis,time,light,temp");
#if ECHO_TO_SERIAL
Serial.println("millis,time,light,temp");
#if ECHO_TO_SERIAL// attempt to write out the header to the file
if (logfile.writeError || !logfile.sync()) {
error("write header");
}
pinMode(redLEDpin, OUTPUT);
pinMode(greenLEDpin, OUTPUT);
// If you want to set the aref to something other than 5v
//analogReference(EXTERNAL);
}
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 63 of 67

Lets look at the first section:
The first important thing is the delay() call, this is what makes the Arduino wait around until its time to take another
reading. If you recall we #defined the delay between readings to be 1000 millseconds (1 second). By having more
delay between readings we can use less power and not fill the card as fast. Its basically a tradeoff how often you want
to read data but for basic long term logging, taking data every second or so will result in plenty of data!
void loop(void)
{
DateTime now;
// delay for the amount of time we want between readings
delay((LOG_INTERVAL -1) - (millis() % LOG_INTERVAL));
digitalWrite(greenLEDpin, HIGH);
// log milliseconds since starting
uint32_t m = millis();
logfile.print(m); // milliseconds since start
logfile.print(", ");
#if ECHO_TO_SERIAL
Serial.print(m); // milliseconds since start
Serial.print(", ");
#endif
// fetch the time
now = RTC.now();
// log time
logfile.print(now.get()); // seconds since 2000
logfile.print(", ");
logfile.print(now.year(), DEC);
logfile.print("/");
logfile.print(now.month(), DEC);
logfile.print("/");
logfile.print(now.day(), DEC);
logfile.print(" ");
logfile.print(now.hour(), DEC);
logfile.print(":");
logfile.print(now.minute(), DEC);
logfile.print(":");
logfile.print(now.second(), DEC);
#if ECHO_TO_SERIAL
Serial.print(now.get()); // seconds since 2000
Serial.print(", ");
Serial.print(now.year(), DEC);
Serial.print("/");
Serial.print(now.month(), DEC);
Serial.print("/");
Serial.print(now.day(), DEC);
Serial.print(" ");
Serial.print(now.hour(), DEC);
Serial.print(":");
Serial.print(now.minute(), DEC);
Serial.print(":");
Serial.print(now.second(), DEC);
#endif //ECHO_TO_SERIAL
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 64 of 67

Then we turn the green LED on, this is useful to tell us that yes we're reading/writing data now.
Next we call millis() to get the 'time since arduino turned on' and log that to the card. It can be handy to have -
especially if you end up not using the RTC.
Then the familiar RTC.now() call to get a snapshot of the time. Once we have that, we write a timestamp (seconods
since 2000) as well as the date in YY/MM/DD HH:MM:SS time format which can easily be recognized by a
spreadsheet. We have both because the nice thing about a timestamp is that its going to montonically increase and
the nice thing about printed out date is its human readable
Log sensor data
Next is the sensor logging code
This code is pretty straight forward, the processing code is snagged from our earlier tutorial. Then we just print() it to
the card with a comma seperating the two
We finish up by turning the green LED off
int photocellReading = analogRead(photocellPin);
delay(10);
int tempReading = analogRead(tempPin);
// converting that reading to voltage, for 3.3v arduino use 3.3
float voltage = (tempReading * 5.0) / 1024.0;
float temperatureC = (voltage - 0.5) * 100.0 ;
float temperatureF = (temperatureC * 9.0 / 5.0) + 32.0;
logfile.print(", ");
logfile.print(photocellReading);
logfile.print(", ");
logfile.println(temperatureF);
#if ECHO_TO_SERIAL
Serial.print(", ");
Serial.print(photocellReading);
Serial.print(", ");
Serial.println(temperatureF);
#endif //ECHO_TO_SERIAL
digitalWrite(greenLEDpin, LOW);
}
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 65 of 67

Downloads
Files
EagleCAD PCB files on GitHub (https://adafru.it/rej)
Fritzing object in Adafruit Fritzing library (https://adafru.it/aP3)
Revision C Schematics & Fabrication Print
© Adafruit Industries https://learn.adafruit.com/adafruit-data-logger-shield Page 66 of 67

Revision B Schematics
click to enlarge
© Adafruit Industries Last Updated: 2018-11-27 10:56:14 PM UTC Page 67 of 67

Original Version Schematics
Click to enlarge